Bluetooth Mesh Firmware Distribution Client Model#

Bluetooth Mesh Firmware Distribution Client Model.

The Bluetooth Mesh Firmware Distribution Client Model is used to transfer new firmware images to Bluetooth Mesh Firmware Distribution Server Model and monitor progress of a firmware update. As a transport layer Bluetooth Mesh BLOB Transfer (MBT) models are in use.

Modules#

sl_btmesh_evt_fw_dist_client_receivers_status

sl_btmesh_evt_fw_dist_client_receivers_list

sl_btmesh_evt_fw_dist_client_receivers_list_end

sl_btmesh_evt_fw_dist_client_capabilities_status

sl_btmesh_evt_fw_dist_client_distribution_status

sl_btmesh_evt_fw_dist_client_upload_status

sl_btmesh_evt_fw_dist_client_fw_status

sl_btmesh_evt_fw_dist_client_upload_complete

sl_btmesh_evt_fw_dist_client_upload_failed

Enumerations#

enum
sl_btmesh_fw_dist_client_upload_phase_idle = 0x0
sl_btmesh_fw_dist_client_upload_phase_transfer_in_progress = 0x1
sl_btmesh_fw_dist_client_upload_phase_transfer_error = 0x2
sl_btmesh_fw_dist_client_upload_phase_transfer_completed = 0x3
}

The Upload Phase of the Firmware Distribution Server.

enum
sl_btmesh_fw_dist_client_dist_upload_type_in_band = 0x0
sl_btmesh_fw_dist_client_dist_upload_type_out_of_band = 0x1
}

The Upload Type of an ongoing or finished upload.

enum
sl_btmesh_fw_dist_client_dist_oob_not_supported = 0x0
sl_btmesh_fw_dist_client_dist_oob_supported = 0x1
}

Distribution Server OOB Support capability values.

enum
sl_btmesh_fw_dist_client_dist_phase_idle = 0x0
sl_btmesh_fw_dist_client_dist_phase_active = 0x1
sl_btmesh_fw_dist_client_dist_phase_transferred = 0x2
sl_btmesh_fw_dist_client_dist_phase_applying = 0x3
sl_btmesh_fw_dist_client_dist_phase_completed = 0x4
sl_btmesh_fw_dist_client_dist_phase_failed = 0x5
sl_btmesh_fw_dist_client_dist_phase_cancelling = 0x6
sl_btmesh_fw_dist_client_dist_phase_suspended = 0x7
}

The Distribution Phase of the Firmware Distribution Server.

Functions#

sl_status_t
sl_btmesh_fw_dist_client_init(uint16_t elem_index)
sl_status_t
sl_btmesh_fw_dist_client_deinit(uint16_t elem_index)
sl_status_t
sl_btmesh_fw_dist_client_setup(uint16_t elem_index, uint16_t appkey_index, uint8_t ttl)
sl_status_t
sl_btmesh_fw_dist_client_setup_upload(uint16_t elem_index, uint16_t server_address, uint8_t ttl, uint16_t timeout_base, sl_bt_uuid_64_t blob_id, uint32_t size, size_t fwid_len, const uint8_t *fwid)
sl_status_t
sl_btmesh_fw_dist_client_set_upload_metadata(uint16_t elem_index, size_t metadata_len, const uint8_t *metadata)
sl_status_t
sl_btmesh_fw_dist_client_get_receivers(uint16_t elem_index, uint16_t dst, uint16_t start_index, uint16_t max_entries)
sl_status_t
sl_btmesh_fw_dist_client_get(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_start_distribution(uint16_t elem_index, uint16_t dst, uint8_t dist_appkey_index, uint8_t dist_ttl, uint16_t dist_timeout_base, uint8_t transfer_mode, uint8_t update_policy, uint16_t fw_list_index, uint16_t group_address, uuid_128 virtual_address)
sl_status_t
sl_btmesh_fw_dist_client_cancel_distribution(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_apply_distribution(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_suspend_distribution(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_add_receivers(uint16_t elem_index, uint16_t dst, size_t nodes_len, const uint8_t *nodes)
sl_status_t
sl_btmesh_fw_dist_client_delete_all_receivers(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_get_capabilities(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_get_upload(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_status_t
sl_btmesh_fw_dist_client_cancel_upload(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_get_fw(uint16_t elem_index, uint16_t dst, size_t fwid_len, const uint8_t *fwid)
sl_status_t
sl_btmesh_fw_dist_client_get_fw_by_index(uint16_t elem_index, uint16_t dst, uint16_t index)
sl_status_t
sl_btmesh_fw_dist_client_delete_fw(uint16_t elem_index, uint16_t dst, size_t fwid_len, const uint8_t *fwid)
sl_status_t
sl_btmesh_fw_dist_client_delete_all_fw(uint16_t elem_index, uint16_t dst)
sl_status_t
sl_btmesh_fw_dist_client_prepare_oob_upload(uint16_t elem_index, size_t fwid_len, const uint8_t *fwid)
sl_status_t
sl_btmesh_fw_dist_client_start_oob_upload(uint16_t elem_index, uint16_t dst, uint16_t appkey_index, uint8_t ttl, size_t uri_len, const uint8_t *uri)
sl_status_t
sl_status_t

Macros#

#define
sl_btmesh_cmd_fw_dist_client_init_id 0x00590028
#define
sl_btmesh_cmd_fw_dist_client_deinit_id 0x01590028
#define
sl_btmesh_cmd_fw_dist_client_setup_id 0x02590028
#define
sl_btmesh_cmd_fw_dist_client_setup_upload_id 0x03590028
#define
sl_btmesh_cmd_fw_dist_client_set_upload_metadata_id 0x04590028
#define
sl_btmesh_cmd_fw_dist_client_get_receivers_id 0x0e590028
#define
sl_btmesh_cmd_fw_dist_client_get_id 0x0d590028
#define
sl_btmesh_cmd_fw_dist_client_start_distribution_id 0x0f590028
#define
sl_btmesh_cmd_fw_dist_client_cancel_distribution_id 0x10590028
#define
sl_btmesh_cmd_fw_dist_client_apply_distribution_id 0x11590028
#define
sl_btmesh_cmd_fw_dist_client_suspend_distribution_id 0x12590028
#define
sl_btmesh_cmd_fw_dist_client_add_receivers_id 0x13590028
#define
sl_btmesh_cmd_fw_dist_client_delete_all_receivers_id 0x14590028
#define
sl_btmesh_cmd_fw_dist_client_get_capabilities_id 0x15590028
#define
sl_btmesh_cmd_fw_dist_client_get_upload_id 0x16590028
#define
sl_btmesh_cmd_fw_dist_client_start_upload_id 0x17590028
#define
sl_btmesh_cmd_fw_dist_client_cancel_upload_id 0x19590028
#define
sl_btmesh_cmd_fw_dist_client_get_fw_id 0x1a590028
#define
sl_btmesh_cmd_fw_dist_client_get_fw_by_index_id 0x1b590028
#define
sl_btmesh_cmd_fw_dist_client_delete_fw_id 0x1c590028
#define
sl_btmesh_cmd_fw_dist_client_delete_all_fw_id 0x1d590028
#define
sl_btmesh_cmd_fw_dist_client_prepare_oob_upload_id 0x1e590028
#define
sl_btmesh_cmd_fw_dist_client_start_oob_upload_id 0x1f590028
#define
sl_btmesh_cmd_fw_dist_client_suspend_upload_id 0x20590028
#define
sl_btmesh_cmd_fw_dist_client_resume_upload_id 0x21590028
#define
sl_btmesh_rsp_fw_dist_client_init_id 0x00590028
#define
sl_btmesh_rsp_fw_dist_client_deinit_id 0x01590028
#define
sl_btmesh_rsp_fw_dist_client_setup_id 0x02590028
#define
sl_btmesh_rsp_fw_dist_client_setup_upload_id 0x03590028
#define
sl_btmesh_rsp_fw_dist_client_set_upload_metadata_id 0x04590028
#define
sl_btmesh_rsp_fw_dist_client_get_receivers_id 0x0e590028
#define
sl_btmesh_rsp_fw_dist_client_get_id 0x0d590028
#define
sl_btmesh_rsp_fw_dist_client_start_distribution_id 0x0f590028
#define
sl_btmesh_rsp_fw_dist_client_cancel_distribution_id 0x10590028
#define
sl_btmesh_rsp_fw_dist_client_apply_distribution_id 0x11590028
#define
sl_btmesh_rsp_fw_dist_client_suspend_distribution_id 0x12590028
#define
sl_btmesh_rsp_fw_dist_client_add_receivers_id 0x13590028
#define
sl_btmesh_rsp_fw_dist_client_delete_all_receivers_id 0x14590028
#define
sl_btmesh_rsp_fw_dist_client_get_capabilities_id 0x15590028
#define
sl_btmesh_rsp_fw_dist_client_get_upload_id 0x16590028
#define
sl_btmesh_rsp_fw_dist_client_start_upload_id 0x17590028
#define
sl_btmesh_rsp_fw_dist_client_cancel_upload_id 0x19590028
#define
sl_btmesh_rsp_fw_dist_client_get_fw_id 0x1a590028
#define
sl_btmesh_rsp_fw_dist_client_get_fw_by_index_id 0x1b590028
#define
sl_btmesh_rsp_fw_dist_client_delete_fw_id 0x1c590028
#define
sl_btmesh_rsp_fw_dist_client_delete_all_fw_id 0x1d590028
#define
sl_btmesh_rsp_fw_dist_client_prepare_oob_upload_id 0x1e590028
#define
sl_btmesh_rsp_fw_dist_client_start_oob_upload_id 0x1f590028
#define
sl_btmesh_rsp_fw_dist_client_suspend_upload_id 0x20590028
#define
sl_btmesh_rsp_fw_dist_client_resume_upload_id 0x21590028

Enumeration Documentation#

sl_btmesh_fw_dist_client_upload_phase_t#

sl_btmesh_fw_dist_client_upload_phase_t

The Upload Phase of the Firmware Distribution Server.

Enumerator
sl_btmesh_fw_dist_client_upload_phase_idle

(0x0) No Upload in progress.

sl_btmesh_fw_dist_client_upload_phase_transfer_in_progress

(0x1) Upload in progress.

sl_btmesh_fw_dist_client_upload_phase_transfer_error

(0x2) Upload or Upload OOB encountered a transfer error.

sl_btmesh_fw_dist_client_upload_phase_transfer_completed

(0x3) Upload or Upload OOB completed successfully.


Definition at line 18179 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_dist_upload_type_t#

sl_btmesh_fw_dist_client_dist_upload_type_t

The Upload Type of an ongoing or finished upload.

Enumerator
sl_btmesh_fw_dist_client_dist_upload_type_in_band

(0x0) In-band upload via BLOB Transfer.

sl_btmesh_fw_dist_client_dist_upload_type_out_of_band

(0x1) Out-of-band upload.


Definition at line 18211 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_dist_oob_t#

sl_btmesh_fw_dist_client_dist_oob_t

Distribution Server OOB Support capability values.

Enumerator
sl_btmesh_fw_dist_client_dist_oob_not_supported

(0x0) Upload OOB not supported.

sl_btmesh_fw_dist_client_dist_oob_supported

(0x1) Upload OOB supported.


Definition at line 18226 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_dist_phase_t#

sl_btmesh_fw_dist_client_dist_phase_t

The Distribution Phase of the Firmware Distribution Server.

Enumerator
sl_btmesh_fw_dist_client_dist_phase_idle

(0x0) No firmware distribution is in progress.

sl_btmesh_fw_dist_client_dist_phase_active

(0x1) Firmware distribution in progress; sending Update Start or BLOB Transfer messages.

sl_btmesh_fw_dist_client_dist_phase_transferred

(0x2) Firmware distribution in progress; BLOB Transfer is complete, waiting for verification. If the Update Policy is Verify Only, the Distribution Server will park here until it receives a Distribution Apply message from the Distribution Client.

sl_btmesh_fw_dist_client_dist_phase_applying

(0x3) Firmware distribution in progress; sending Update Apply messages.

sl_btmesh_fw_dist_client_dist_phase_completed

(0x4) Firmware distribution completed successfully for at least one Target Node.

sl_btmesh_fw_dist_client_dist_phase_failed

(0x5) Firmware distribution failed for all Target Nodes.

sl_btmesh_fw_dist_client_dist_phase_cancelling

(0x6) Cancelling firmware distribution.

sl_btmesh_fw_dist_client_dist_phase_suspended

(0x7) Firmware distribution is temporarily suspended.


Definition at line 18237 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Function Documentation#

sl_btmesh_fw_dist_client_init#

sl_status_t sl_btmesh_fw_dist_client_init (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

Initialize the Firmware Distribution Client model. An MBT Client on the same element must have been initialized prior to making this call.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 18592 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_deinit#

sl_status_t sl_btmesh_fw_dist_client_deinit (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

Deinitialize the Firmware Distribution Client model. The corresponding MBT Client instance can be deinitialized before or after the Distribution Client.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 18604 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_setup#

sl_status_t sl_btmesh_fw_dist_client_setup (uint16_t elem_index, uint16_t appkey_index, uint8_t ttl)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]appkey_index

Application key index

uint8_t[in]ttl

The time-to-live value to use. Valid values: 0, range:[2-127] and 255.

Set up the communication parameters for a Distribution Client instance.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 18618 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_setup_upload#

sl_status_t sl_btmesh_fw_dist_client_setup_upload (uint16_t elem_index, uint16_t server_address, uint8_t ttl, uint16_t timeout_base, sl_bt_uuid_64_t blob_id, uint32_t size, size_t fwid_len, const uint8_t * fwid)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]server_address

Address of the target Distributor

uint8_t[in]ttl

The time-to-live value to use for the upload. Valid values: 0, range:[2-127] and 255.

uint16_t[in]timeout_base

Timeout Base value for the BLOB Transfer

sl_bt_uuid_64_t[in]blob_id

BLOB ID to use

uint32_t[in]size

Size of the firmware image

size_t[in]fwid_len

Length of data in fwid

const uint8_t *[in]fwid

Firmware ID of the firmware image

Set up an in-band Upload of a firmware image. Note that only one upload can be executed at a time. This command must be used before setting the upload image metadata via sl_btmesh_fw_dist_client_set_upload_metadata.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 18641 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_set_upload_metadata#

sl_status_t sl_btmesh_fw_dist_client_set_upload_metadata (uint16_t elem_index, size_t metadata_len, const uint8_t * metadata)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

size_t[in]metadata_len

Length of data in metadata

const uint8_t *[in]metadata

Metadata for the firmware image

Set the metadata for an in-band Upload of a firmware image.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 18661 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get_receivers#

sl_status_t sl_btmesh_fw_dist_client_get_receivers (uint16_t elem_index, uint16_t dst, uint16_t start_index, uint16_t max_entries)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

uint16_t[in]start_index

Starting index of node statuses to request

uint16_t[in]max_entries

Maximum number of node statuses to request

Send a Receivers Get message. This function is used to get a slice of the Receivers List on the Distribution Server. The response is a Receivers List message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18683 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get#

sl_status_t sl_btmesh_fw_dist_client_get (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Distribution Get message. This function is used to determine the parameters of an ongoing distribution, if any. The response is a Distribution Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18703 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_start_distribution#

sl_status_t sl_btmesh_fw_dist_client_start_distribution (uint16_t elem_index, uint16_t dst, uint8_t dist_appkey_index, uint8_t dist_ttl, uint16_t dist_timeout_base, uint8_t transfer_mode, uint8_t update_policy, uint16_t fw_list_index, uint16_t group_address, uuid_128 virtual_address)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

uint8_t[in]dist_appkey_index

Application key to use for the communication between the Distributor and Target Nodes

uint8_t[in]dist_ttl

The time-to-live value for the Distributor to use when communicating with the Target Nodes. Valid values: 0, range:[2-127] and 255

uint16_t[in]dist_timeout_base

The Timeout Base value to use in the firmware image BLOB Transfer

uint8_t[in]transfer_mode

1 = use Push Mode, 2 = use Pull Mode (typically for LPNs)

uint8_t[in]update_policy

Enum sl_btmesh_fw_dist_server_dfu_policy_t. 0 = Verify Only (Initiator sends Distribution Apply to Distributor to apply the update), 1 = Verify and Apply (Distributor applies update automatically)

uint16_t[in]fw_list_index

Index of the firmware image in the Distributor's Firmware List

uint16_t[in]group_address

Group address to use. Zero to only use unicast.

uuid_128[in]virtual_address

If the group address is a VA hash, this needs to contain the full virtual address label UUID. Otherwise, the value of this field will be ignored.

Send a Distribution Start message. This function is used to start a new distribution process. The Receivers List must have been populated via sl_btmesh_fw_dist_client_add_receivers, and the firmware image must have been uploaded to the Distribution Server. The response is a Distribution Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18739 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_cancel_distribution#

sl_status_t sl_btmesh_fw_dist_client_cancel_distribution (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Distribution Cancel message. This function is used to cancel a distribution process. The response is a Distribution Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18764 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_apply_distribution#

sl_status_t sl_btmesh_fw_dist_client_apply_distribution (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Distribution Apply message. This function is used to trigger applying the firmware update on the Target Nodes. This should only be used if the Update Policy of the distribution is Verify Only. The response is a Distribution Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18783 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_suspend_distribution#

sl_status_t sl_btmesh_fw_dist_client_suspend_distribution (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Distribution Suspend message. This function is used to suspend a distribution when the BLOB Transfer is still in progress. It cannot be used after the image has already been fully transferred. The response is a Distribution Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18802 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_add_receivers#

sl_status_t sl_btmesh_fw_dist_client_add_receivers (uint16_t elem_index, uint16_t dst, size_t nodes_len, const uint8_t * nodes)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

size_t[in]nodes_len

Length of data in nodes

const uint8_t *[in]nodes

List of (address [uint16], fw_index [uint8]) pairs.

Send a Receivers Add message. This function is used to add Target Nodes to the Distribution Server's Receivers List. The response is a Receivers Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18822 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_delete_all_receivers#

sl_status_t sl_btmesh_fw_dist_client_delete_all_receivers (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Receivers Delete All message. This function is used to clear the Receivers List on the Distribution Server. The response is a Receivers Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18842 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get_capabilities#

sl_status_t sl_btmesh_fw_dist_client_get_capabilities (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Capabilities Get message. This function is used to determine the Distribution Capabilities of a Distribution Server. The response is a Capabilities Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18860 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get_upload#

sl_status_t sl_btmesh_fw_dist_client_get_upload (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send an Upload Get message. This function is used to check if an upload is ongoing, and what its progress is. The response is an Upload Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18877 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_start_upload#

sl_status_t sl_btmesh_fw_dist_client_start_upload (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

Start an upload previously set up with sl_btmesh_fw_dist_client_setup_upload. Calling this function will send an Upload Start message. The response is an Upload Status message. Note that if the remote end does not respond, this function may need to be retried. Note that upon sending the Upload Start message a response timer is started for a time frame of: (10000 * (timeout_base + 2)) + (100 * ttl) in units of ms.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18898 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_cancel_upload#

sl_status_t sl_btmesh_fw_dist_client_cancel_upload (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Cancel an upload previously started with sl_btmesh_fw_dist_client_start_upload.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18914 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get_fw#

sl_status_t sl_btmesh_fw_dist_client_get_fw (uint16_t elem_index, uint16_t dst, size_t fwid_len, const uint8_t * fwid)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

size_t[in]fwid_len

Length of data in fwid

const uint8_t *[in]fwid

Firmware ID of the firmware image

Send a Firmware Get message. This function is used to check if a firmware image with the given FWID exists on the Distribution Server, and if it does, to retrieve its Firmware List Index. The response is a Firmware Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18935 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_get_fw_by_index#

sl_status_t sl_btmesh_fw_dist_client_get_fw_by_index (uint16_t elem_index, uint16_t dst, uint16_t index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

uint16_t[in]index

Index to check

Send a Firmware Get By Index message. This function is used to check if a firmware with a particular index exists on the Distribution Server, and if it does, to retrieve its FWID. The response is a Firmware Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18956 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_delete_fw#

sl_status_t sl_btmesh_fw_dist_client_delete_fw (uint16_t elem_index, uint16_t dst, size_t fwid_len, const uint8_t * fwid)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

size_t[in]fwid_len

Length of data in fwid

const uint8_t *[in]fwid

Firmware ID of the firmware image

Send a Firmware Delete message. This function is used to delete a particular firmware on the Distribution Server. The response is a Firmware Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18977 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_delete_all_fw#

sl_status_t sl_btmesh_fw_dist_client_delete_all_fw (uint16_t elem_index, uint16_t dst)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Address of the Distributor

Send a Firmware Delete All message. This function is used to delete all firmware images on the Distribution Server. The response is a Firmware Status message.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 18997 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_prepare_oob_upload#

sl_status_t sl_btmesh_fw_dist_client_prepare_oob_upload (uint16_t elem_index, size_t fwid_len, const uint8_t * fwid)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

size_t[in]fwid_len

Length of data in fwid

const uint8_t *[in]fwid

FWID used to form the query string for the Distribution Server's Check Firmware OOB and Store Firmware OOB procedures.

Prepare an OOB Upload. This must be called before calling the sl_btmesh_fw_dist_client_start_oob_upload command. Calling this multiple times will overwrite the state of the previous OOB Upload.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19014 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_start_oob_upload#

sl_status_t sl_btmesh_fw_dist_client_start_oob_upload (uint16_t elem_index, uint16_t dst, uint16_t appkey_index, uint8_t ttl, size_t uri_len, const uint8_t * uri)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

uint16_t[in]dst

Destination address

uint16_t[in]appkey_index

Application key index to use for encrypting the message.

uint8_t[in]ttl

The time-to-live value to use. Valid values: 0, range:[2-127] and 255.

size_t[in]uri_len

Length of data in uri

const uint8_t *[in]uri

URI used to form the query string for the Distribution Server's Check Firmware OOB and Store Firmware OOB procedures.

Start an OOB Upload. The response is an sl_btmesh_evt_fw_dist_client_upload_status event. This command must be repeated by the application if the remote end does not respond. If the event's status field is zero, the request was accepted; otherwise it was rejected. If the event indicates that the request was accepted, the type field will be set to 1 to denote an out-of-band upload.

sl_btmesh_fw_dist_client_prepare_oob_upload must have been called prior to using this command.

To poll the status of the OOB Upload, the application can either repeat this command, or use the command sl_btmesh_fw_dist_client_get_upload.

When a sl_btmesh_evt_fw_dist_client_upload_status event with type set to 1 and progress set to 100 is received, the application can consider the upload complete.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 19053 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_suspend_upload#

sl_status_t sl_btmesh_fw_dist_client_suspend_upload (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

Suspend an Upload's BLOB Transfer. An Upload that isn't yet in the BLOB Transfer phase, or which has failed, cannot be suspended. The suspension is entirely local; there is no message sent over the air. The remote receiver's BLOB Transfer Server will go to the suspended phase when the Upload Timeout timer expires. When the Upload is resumed, it will continue from where it previously left off.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19074 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_fw_dist_client_resume_upload#

sl_status_t sl_btmesh_fw_dist_client_resume_upload (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Client model element index

Resume a suspended upload. The command sl_btmesh_fw_dist_client_start_upload must be used after this command, and it may need to be repeated if the remote end does not respond. When the Upload is resumed, the BLOB Transfer will continue from where it previously left off.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19089 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h