Bluetooth Mesh Generic Server Model#

Bluetooth Mesh Generic Server Model.

Generic server model API provides functionality to send and receive messages using Bluetooth SIG server models, including generic server models and lighting server models.

Throughout the API the server model being used is identified by its element address and model ID, while the client model generating requests to the server model is identified by its element address and model ID.

The generic server model API is designed on the premise that the actual state the model represents resides in and is owned by the application, not by the stack.

The model acts as a cache for client queries. In other words, the stack handles state requests from the client automatically. The application does not need to handle those. The cached value is also used for periodic publication.

The flip side of caching is that when the state represented by the model changes in the application, it must update the cached value to the stack by issuing a sl_btmesh_generic_server_update command.

When a client model requests a state change, the stack will generate a sl_btmesh_evt_generic_server_client_request event which the application must process. Then, if the client needs a response the application has to issue a sl_btmesh_generic_server_respond command corresponding to the request. Otherwise, the application only has to update the state with a sl_btmesh_generic_server_update command, which does not result in sending any messages to the network.

Note that, because the Mesh Model specification requires that certain states are bound together and because the stack enforces that, updating one cached state may result in an update of the corresponding bound state, for which the stack generates a sl_btmesh_evt_generic_server_state_changed event. For example, when a dimmable light is switched off, the lightness level bound to the on/off state, is also set to zero because the states are bound.

Data for state change requests and server responses is passed as serialized byte arrays through BGAPI. Bluetooth mesh SDK has functions to convert byte arrays to and from model state structures.

The stack will handle Mesh transaction layer segmentation and reassembly automatically if the messages sent are long enough to require it.

Note on time resolution

Because of message formatting, transition time and remaining time resolution units depend on the requested or reported value. For example, until 6.2 seconds it is 100 ms; until 62 seconds it is 1 s; until 620 seconds it is 10 s; and until 620 minutes it is 10 minutes. The value can't be longer than 620 minutes. Therefore, it is not possible to request a delay of exactly 7500 ms. The resolution unit is 1 s between 6.2 and 62 seconds, so the value is rounded down to 7 s.

Delay resolution is 5 ms and values will be rounded down to the closest 5 ms. The value can't be longer than 1275 ms.

Modules#

sl_btmesh_evt_generic_server_client_request

sl_btmesh_evt_generic_server_state_changed

sl_btmesh_evt_generic_server_state_recall

Functions#

sl_status_t
sl_btmesh_generic_server_respond(uint16_t client_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint32_t remaining_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t *parameters)
sl_status_t
sl_btmesh_generic_server_update(uint16_t elem_index, uint16_t model_id, uint32_t remaining_ms, uint8_t type, size_t parameters_len, const uint8_t *parameters)
sl_status_t
sl_btmesh_generic_server_publish(uint16_t elem_index, uint16_t model_id, uint8_t type)
sl_status_t
sl_btmesh_generic_server_get_cached_state(uint16_t elem_index, uint16_t model_id, uint8_t type, uint32_t *remaining_ms, size_t max_parameters_size, size_t *parameters_len, uint8_t *parameters)

Macros#

Function Documentation#

sl_btmesh_generic_server_respond#

sl_status_t sl_btmesh_generic_server_respond (uint16_t client_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint32_t remaining_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t * parameters)
Parameters
[in]client_address

Address of the client model which sent the message

[in]elem_index

Server model element index

[in]model_id

Server model ID

[in]appkey_index

The application key index used

[in]remaining_ms

Time (in milliseconds) remaining before transition from current state to target state is complete. Set to zero if no transition is taking place or if the transition time does not apply to the state change.

[in]flags

Message flags. Bitmask of the following:

  • Bit 0: Non-relayed. If non-zero, indicates a response to a non-relayed request.

[in]type

Model-specific state type, identifying the kind of state to be updated. See Generic Client Get State Types list for details.

[in]parameters_len

Length of data in parameters

[in]parameters

Message-specific parameters serialized into a byte array

Server response to a client request. This command must be used when an application updates the server model state as a response to a sl_btmesh_evt_generic_server_client_request event which required a response.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5902 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_update#

sl_status_t sl_btmesh_generic_server_update (uint16_t elem_index, uint16_t model_id, uint32_t remaining_ms, uint8_t type, size_t parameters_len, const uint8_t * parameters)
Parameters
[in]elem_index

Server model element index

[in]model_id

Server model ID

[in]remaining_ms

Time (in milliseconds) remaining before transition from current state to target state is complete. Set to zero if no transition is taking place or if transition time does not apply to the state change.

[in]type

Model-specific state type, identifying the kind of state to be updated. See Generic Client Get State Types list for details.

[in]parameters_len

Length of data in parameters

[in]parameters

Message-specific parameters, serialized into a byte array

Server state update. This command must be used when an application updates the server model state as a response to a sl_btmesh_evt_generic_server_client_request event which did not require a response, but also when the application state changes spontaneously or as a result of some external (non-Mesh) event.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5936 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_publish#

sl_status_t sl_btmesh_generic_server_publish (uint16_t elem_index, uint16_t model_id, uint8_t type)
Parameters
[in]elem_index

Server model element index

[in]model_id

Server model ID

[in]type

Model-specific state type, identifying the kind of state used in the published message. See Generic Client Get State Types list for details.

Publish the server state to the network using the publish parameters configured in the model. The message is constructed using the cached state in the stack.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5958 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init#

sl_status_t sl_btmesh_generic_server_init ()

Initialize generic server models. This command initializes all generic server models on the device. Alternatively, only the necessary server models can be initialized using model-specific initialization commands. Using model-specific initialization can result in a smaller firmware image size for SoC projects.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5974 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_common#

sl_status_t sl_btmesh_generic_server_init_common ()

Initialize the generic server model common functionality. This should be called after all model-specific initialization calls are done, and does not need to be called if sl_btmesh_generic_server_init is used.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5986 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_on_off#

sl_status_t sl_btmesh_generic_server_init_on_off ()

Initialize generic on/off server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5996 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_level#

sl_status_t sl_btmesh_generic_server_init_level ()

Initialize generic level server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6006 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_default_transition_time#

sl_status_t sl_btmesh_generic_server_init_default_transition_time ()

Initialize generic default transition time server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6016 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_power_on_off#

sl_status_t sl_btmesh_generic_server_init_power_on_off ()

Initialize generic power on/off server models, power on/off setup server models, and all models they extend.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6027 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_power_level#

sl_status_t sl_btmesh_generic_server_init_power_level ()

Initialize generic power level server models, power level setup server models, and all models they extend.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6038 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_battery#

sl_status_t sl_btmesh_generic_server_init_battery ()

Initialize generic battery server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6048 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_location#

sl_status_t sl_btmesh_generic_server_init_location ()

Initialize generic location and generic location setup server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6058 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_property#

sl_status_t sl_btmesh_generic_server_init_property ()

Initialize generic property server models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6068 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_lightness#

sl_status_t sl_btmesh_generic_server_init_lightness ()

Initialize light lightness server models, light lightness setup server models, and all models they extend.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6079 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_ctl#

sl_status_t sl_btmesh_generic_server_init_ctl ()

Initialize light CTL server models, light CTL temperature server models, light CTL setup server models, and all models they extend.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6090 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_init_hsl#

sl_status_t sl_btmesh_generic_server_init_hsl ()

Initialize light HSL server models, light HSL hue server models, light HSL saturation server models, light HSL setup server models, and all models they extend

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6102 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_server_get_cached_state#

sl_status_t sl_btmesh_generic_server_get_cached_state (uint16_t elem_index, uint16_t model_id, uint8_t type, uint32_t * remaining_ms, size_t max_parameters_size, size_t * parameters_len, uint8_t * parameters)
Parameters
[in]elem_index

Server model element index

[in]model_id

Server model ID

[in]type

Model-specific state type, identifying the kind of state reported in the state change event. See Generic Client Get State Types list for details.

[out]remaining_ms

Time (in milliseconds) remaining before transition from current state to target state is complete. Ignored if no transition is taking place.

[in]max_parameters_size

Size of output buffer passed in parameters

[out]parameters_len

On return, set to the length of output data written to parameters

[out]parameters

Message-specific parameters, serialized into a byte array

Get model cached state. This command can be used to get cached model states after scene recall when using compacted recall events. This command supports only those states that would have been reported by sl_btmesh_evt_generic_server_state_recall events.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 6128 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_cmd_generic_server_respond_id#

#define sl_btmesh_cmd_generic_server_respond_id
Value:
0x001f0028

Definition at line 5708 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_update_id#

#define sl_btmesh_cmd_generic_server_update_id
Value:
0x011f0028

Definition at line 5709 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_publish_id#

#define sl_btmesh_cmd_generic_server_publish_id
Value:
0x021f0028

Definition at line 5710 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_id#

#define sl_btmesh_cmd_generic_server_init_id
Value:
0x041f0028

Definition at line 5711 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_common_id#

#define sl_btmesh_cmd_generic_server_init_common_id
Value:
0x051f0028

Definition at line 5712 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_on_off_id#

#define sl_btmesh_cmd_generic_server_init_on_off_id
Value:
0x061f0028

Definition at line 5713 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_level_id#

#define sl_btmesh_cmd_generic_server_init_level_id
Value:
0x071f0028

Definition at line 5714 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_default_transition_time_id#

#define sl_btmesh_cmd_generic_server_init_default_transition_time_id
Value:
0x081f0028

Definition at line 5715 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_power_on_off_id#

#define sl_btmesh_cmd_generic_server_init_power_on_off_id
Value:
0x091f0028

Definition at line 5716 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_power_level_id#

#define sl_btmesh_cmd_generic_server_init_power_level_id
Value:
0x0a1f0028

Definition at line 5717 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_battery_id#

#define sl_btmesh_cmd_generic_server_init_battery_id
Value:
0x0b1f0028

Definition at line 5718 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_location_id#

#define sl_btmesh_cmd_generic_server_init_location_id
Value:
0x0c1f0028

Definition at line 5719 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_property_id#

#define sl_btmesh_cmd_generic_server_init_property_id
Value:
0x0d1f0028

Definition at line 5720 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_lightness_id#

#define sl_btmesh_cmd_generic_server_init_lightness_id
Value:
0x0e1f0028

Definition at line 5721 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_ctl_id#

#define sl_btmesh_cmd_generic_server_init_ctl_id
Value:
0x0f1f0028

Definition at line 5722 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_init_hsl_id#

#define sl_btmesh_cmd_generic_server_init_hsl_id
Value:
0x101f0028

Definition at line 5723 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_generic_server_get_cached_state_id#

#define sl_btmesh_cmd_generic_server_get_cached_state_id
Value:
0x111f0028

Definition at line 5724 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_respond_id#

#define sl_btmesh_rsp_generic_server_respond_id
Value:
0x001f0028

Definition at line 5725 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_update_id#

#define sl_btmesh_rsp_generic_server_update_id
Value:
0x011f0028

Definition at line 5726 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_publish_id#

#define sl_btmesh_rsp_generic_server_publish_id
Value:
0x021f0028

Definition at line 5727 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_id#

#define sl_btmesh_rsp_generic_server_init_id
Value:
0x041f0028

Definition at line 5728 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_common_id#

#define sl_btmesh_rsp_generic_server_init_common_id
Value:
0x051f0028

Definition at line 5729 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_on_off_id#

#define sl_btmesh_rsp_generic_server_init_on_off_id
Value:
0x061f0028

Definition at line 5730 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_level_id#

#define sl_btmesh_rsp_generic_server_init_level_id
Value:
0x071f0028

Definition at line 5731 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_default_transition_time_id#

#define sl_btmesh_rsp_generic_server_init_default_transition_time_id
Value:
0x081f0028

Definition at line 5732 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_power_on_off_id#

#define sl_btmesh_rsp_generic_server_init_power_on_off_id
Value:
0x091f0028

Definition at line 5733 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_power_level_id#

#define sl_btmesh_rsp_generic_server_init_power_level_id
Value:
0x0a1f0028

Definition at line 5734 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_battery_id#

#define sl_btmesh_rsp_generic_server_init_battery_id
Value:
0x0b1f0028

Definition at line 5735 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_location_id#

#define sl_btmesh_rsp_generic_server_init_location_id
Value:
0x0c1f0028

Definition at line 5736 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_property_id#

#define sl_btmesh_rsp_generic_server_init_property_id
Value:
0x0d1f0028

Definition at line 5737 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_lightness_id#

#define sl_btmesh_rsp_generic_server_init_lightness_id
Value:
0x0e1f0028

Definition at line 5738 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_ctl_id#

#define sl_btmesh_rsp_generic_server_init_ctl_id
Value:
0x0f1f0028

Definition at line 5739 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_init_hsl_id#

#define sl_btmesh_rsp_generic_server_init_hsl_id
Value:
0x101f0028

Definition at line 5740 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_generic_server_get_cached_state_id#

#define sl_btmesh_rsp_generic_server_get_cached_state_id
Value:
0x111f0028

Definition at line 5741 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h