Bluetooth Mesh Generic Client Model#

Bluetooth Mesh Generic Client Model.

Generic client model API provides a functionality to send and receive messages using Bluetooth SIG client models, including generic client models and lighting client models.

In the API, the client model that is used is identified by its element address and model ID, while the server model responding to client model requests is identified by its element address and model ID.

The API has functions for querying server model states, requesting server model state changes, and publishing messages. The application has to implement more complex functionality (state machines or other model-specific logic).

Data for state change requests and server responses is passed as serialized byte arrays through BGAPI. There are functions to convert byte arrays to and from model state structures in the Bluetooth mesh SDK.

The stack will handle Mesh transaction layer segmentation and reassembly automatically if the messages sent are long enough to require it.

Note on time resolution

Because of message formatting, transition time and remaining time resolution units depend on the requested or reported value. For example, until 6.2 seconds it is 100 ms; until 62 seconds it is 1 s; until 620 seconds it is 10 s; and until 620 minutes it is 10 minutes. The value cannot be longer than 620 minutes. Therefore, it is not possible to request a delay of exactly 7500 ms. The resolution unit is 1 s between 6.2 and 62 seconds, so the value would be rounded down to 7 s.

Delay resolution is 5 ms and values will be rounded down to the closest 5 ms. The value can't be longer than 1275 ms.

Modules#

Generic Client Get State Types

Generic Client Set Request Types

sl_btmesh_evt_generic_client_server_status

Functions#

sl_status_t
sl_btmesh_generic_client_get(uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type)
sl_status_t
sl_btmesh_generic_client_set(uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t *parameters)
sl_status_t
sl_btmesh_generic_client_publish(uint16_t elem_index, uint16_t model_id, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t *parameters)
sl_status_t
sl_btmesh_generic_client_get_params(uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type, size_t parameters_len, const uint8_t *parameters)

Macros#

#define
sl_btmesh_cmd_generic_client_get_id 0x001e0028
#define
sl_btmesh_cmd_generic_client_set_id 0x011e0028
#define
sl_btmesh_cmd_generic_client_publish_id 0x021e0028
#define
sl_btmesh_cmd_generic_client_get_params_id 0x031e0028
#define
sl_btmesh_cmd_generic_client_init_id 0x041e0028
#define
sl_btmesh_cmd_generic_client_init_common_id 0x051e0028
#define
sl_btmesh_cmd_generic_client_init_on_off_id 0x061e0028
#define
sl_btmesh_cmd_generic_client_init_level_id 0x071e0028
#define
sl_btmesh_cmd_generic_client_init_default_transition_time_id 0x081e0028
#define
sl_btmesh_cmd_generic_client_init_power_on_off_id 0x091e0028
#define
sl_btmesh_cmd_generic_client_init_power_level_id 0x0a1e0028
#define
sl_btmesh_cmd_generic_client_init_battery_id 0x0b1e0028
#define
sl_btmesh_cmd_generic_client_init_location_id 0x0c1e0028
#define
sl_btmesh_cmd_generic_client_init_property_id 0x0d1e0028
#define
sl_btmesh_cmd_generic_client_init_lightness_id 0x0e1e0028
#define
sl_btmesh_cmd_generic_client_init_ctl_id 0x0f1e0028
#define
sl_btmesh_cmd_generic_client_init_hsl_id 0x101e0028
#define
sl_btmesh_rsp_generic_client_get_id 0x001e0028
#define
sl_btmesh_rsp_generic_client_set_id 0x011e0028
#define
sl_btmesh_rsp_generic_client_publish_id 0x021e0028
#define
sl_btmesh_rsp_generic_client_get_params_id 0x031e0028
#define
sl_btmesh_rsp_generic_client_init_id 0x041e0028
#define
sl_btmesh_rsp_generic_client_init_common_id 0x051e0028
#define
sl_btmesh_rsp_generic_client_init_on_off_id 0x061e0028
#define
sl_btmesh_rsp_generic_client_init_level_id 0x071e0028
#define
sl_btmesh_rsp_generic_client_init_default_transition_time_id 0x081e0028
#define
sl_btmesh_rsp_generic_client_init_power_on_off_id 0x091e0028
#define
sl_btmesh_rsp_generic_client_init_power_level_id 0x0a1e0028
#define
sl_btmesh_rsp_generic_client_init_battery_id 0x0b1e0028
#define
sl_btmesh_rsp_generic_client_init_location_id 0x0c1e0028
#define
sl_btmesh_rsp_generic_client_init_property_id 0x0d1e0028
#define
sl_btmesh_rsp_generic_client_init_lightness_id 0x0e1e0028
#define
sl_btmesh_rsp_generic_client_init_ctl_id 0x0f1e0028
#define
sl_btmesh_rsp_generic_client_init_hsl_id 0x101e0028

Function Documentation#

sl_btmesh_generic_client_get#

sl_status_t sl_btmesh_generic_client_get (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type)
Parameters
[in]server_address

Destination server model address

[in]elem_index

Client model element index

[in]model_id

Client model ID

[in]appkey_index

The application key index to use

[in]type

Model-specific state type, identifying the kind of state to retrieve. See Generic Client Get State Types list for details.

Get the current state of a server model or models in the network. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.

The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 5345 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_set#

sl_status_t sl_btmesh_generic_client_set (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t * parameters)
Parameters
[in]server_address

Destination server model address

[in]elem_index

Client model element index

[in]model_id

Client model ID

[in]appkey_index

The application key index to use

[in]tid

Transaction identifier. This applies to those messages the Mesh Model specification defines as transactional and can be left as zero for others.

[in]transition_ms

Transition time (in milliseconds) for the state change. If both the transition time and the delay are zero, the transition is immediate.

This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others.

[in]delay_ms

Delay time (in milliseconds) before starting the state change. If both the transition time and the delay are zero, the transition is immediate.

This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others.

[in]flags

Message flags. Bitmask of the following:

  • Bit 0: Response required. If non-zero, the client expects a response from the server

  • Bit 1: Default transition timer. If non-zero, the client requests that server uses its default transition timer and the supplied transition and delay values are ignored.

[in]type

Model-specific request type. See set request types list for details.

[in]parameters_len

Length of data in parameters

[in]parameters

Message-specific set request parameters serialized into a byte array

Set the current state of a server model or models in the network. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.

The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events. Note that for responses to be generated the corresponding flag needs to be set.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 5400 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_publish#

sl_status_t sl_btmesh_generic_client_publish (uint16_t elem_index, uint16_t model_id, uint8_t tid, uint32_t transition_ms, uint16_t delay_ms, uint16_t flags, uint8_t type, size_t parameters_len, const uint8_t * parameters)
Parameters
[in]elem_index

Client model element index

[in]model_id

Client model ID

[in]tid

Transaction identifier

[in]transition_ms

Transition time (in milliseconds) for the state change. If both the transition time and the delay are zero, the transition is immediate.

This applies to messages the Mesh Model specification defines to have transition and delay times and can be left as zero for others.

[in]delay_ms

Delay time (in milliseconds) before starting the state change. If both the transition time and the delay are zero, the transition is immediate.

This applies to messages the Mesh Model specification defines to have transition and delay times, and can be left as zero for others.

[in]flags

Message flags. Bitmask of the following:

  • Bit 0: Response required. If non-zero, the client expects a response from the server

  • Bit 1: Default transition timer. If non-zero client requests that server uses its default transition timer and the supplied transition and delay values are ignored.

[in]type

Model-specific request type. See set request types list for details.

[in]parameters_len

Length of data in parameters

[in]parameters

Message-specific set request parameters serialized into a byte array

Publish a set request to the network using the publish address and publish application key of the model. The message will be received by the server models which subscribe to the publish address, and there's no need to explicitly specify a destination address or application key.

The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events. To generate responses, the corresponding flag needs to be set.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 5458 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_get_params#

sl_status_t sl_btmesh_generic_client_get_params (uint16_t server_address, uint16_t elem_index, uint16_t model_id, uint16_t appkey_index, uint8_t type, size_t parameters_len, const uint8_t * parameters)
Parameters
[in]server_address

Destination server model address

[in]elem_index

Client model element index

[in]model_id

Client model ID

[in]appkey_index

The application key index to use.

[in]type

Model-specific state type, identifying the kind of state to retrieve. See Generic Client Get State Types list for details.

[in]parameters_len

Length of data in parameters

[in]parameters

Message-specific get request parameters serialized into a byte array

Get the current state of a server model or models in the network, with additional parameters detailing the request. Besides the immediate result code, the response or responses from the network will generate server state report events for the replies received.

The server model responses will be reported in sl_btmesh_evt_generic_client_server_status events.

This call is used to query properties, for which the property ID is given as a parameter.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 5498 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init#

sl_status_t sl_btmesh_generic_client_init ()

Initialize generic client models. This command initializes all generic client models on the device. Alternatively, only the necessary client models can be initialized using model-specific initialization commands. Using model-specific initialization can result in a smaller firmware image size for SoC projects.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5518 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_common#

sl_status_t sl_btmesh_generic_client_init_common ()

Initialize the generic client model common functionality. This command should be called after all model-specific initialization calls are done. It does not need to be called if sl_btmesh_generic_client_init is used.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5530 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_on_off#

sl_status_t sl_btmesh_generic_client_init_on_off ()

Initialize generic on/off client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5540 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_level#

sl_status_t sl_btmesh_generic_client_init_level ()

Initialize generic level client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5550 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_default_transition_time#

sl_status_t sl_btmesh_generic_client_init_default_transition_time ()

Initialize generic default transition time client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5560 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_power_on_off#

sl_status_t sl_btmesh_generic_client_init_power_on_off ()

Initialize generic power on/off client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5570 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_power_level#

sl_status_t sl_btmesh_generic_client_init_power_level ()

Initialize generic power level client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5580 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_battery#

sl_status_t sl_btmesh_generic_client_init_battery ()

Initialize generic battery client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5590 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_location#

sl_status_t sl_btmesh_generic_client_init_location ()

Initialize generic location client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5600 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_property#

sl_status_t sl_btmesh_generic_client_init_property ()

Initialize generic property client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5610 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_lightness#

sl_status_t sl_btmesh_generic_client_init_lightness ()

Initialize light lightness client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5620 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_ctl#

sl_status_t sl_btmesh_generic_client_init_ctl ()

Initialize light CTL client models.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5630 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_generic_client_init_hsl#

sl_status_t sl_btmesh_generic_client_init_hsl ()

Initialize light HSL client models

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 5640 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h