Generic Client Set Request Types#
Generic client set request type identifies the state which the client requests to be set to a new value on the remote server model.
Macros#
Macro Definition Documentation#
SL_BTMESH_GENERIC_CLIENT_REQUEST_ON_OFF#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_ON_OFFValue:
0x0
Generic on/off set request
5190
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_ON_POWER_UP#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_ON_POWER_UPValue:
0x1
Generic on power up set request
5193
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVELValue:
0x2
Generic level set request
5196
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_DELTA#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_DELTAValue:
0x3
Generic level delta set request
5199
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_MOVE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_MOVEValue:
0x4
Generic level move set request
5202
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_HALT#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LEVEL_HALTValue:
0x5
Generic level halt request
5205
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVEL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVELValue:
0x6
Generic power level set request
5208
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVEL_DEFAULT#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVEL_DEFAULTValue:
0x7
Generic power level default set request
5211
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVEL_RANGE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_POWER_LEVEL_RANGEValue:
0x8
Generic power level range set request
5214
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_TRANSITION_TIME#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_TRANSITION_TIMEValue:
0x9
Generic transition time set request
5217
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LOCATION_GLOBAL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LOCATION_GLOBALValue:
0xa
Generic global location set request
5220
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LOCATION_LOCAL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LOCATION_LOCALValue:
0xb
Generic local location set request
5223
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_USER#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_USERValue:
0xc
Generic user property set request
5226
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_ADMIN#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_ADMINValue:
0xd
Generic admin property set request
5229
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_MANUF#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_PROPERTY_MANUFValue:
0xe
Generic manufacturer property set request
5232
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_ACTUAL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_ACTUALValue:
0x80
Light actual lightness set request
5235
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_LINEAR#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_LINEARValue:
0x81
Light linear lightness set request
5238
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_DEFAULT#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_DEFAULTValue:
0x82
Light default lightness set request
5241
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_RANGE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_LIGHTNESS_RANGEValue:
0x83
Light lightness range set request
5244
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_CTLValue:
0x84
Light lightness, color temperature, and delta UV set request
5247
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_TEMPERATURE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_TEMPERATUREValue:
0x85
Light color temperature and delta UV set request
5250
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_DEFAULT#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_DEFAULTValue:
0x86
Light lightness, color temperature, and delta UV default set request
5253
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_RANGE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_CTL_RANGEValue:
0x87
Light color temperature range set request
5256
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_HSLValue:
0x88
Light lightness, color hue, and color saturation set request
5259
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_HUE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_HUEValue:
0x89
Light color hue set request
5262
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_SATURATION#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_SATURATIONValue:
0x8a
Light color saturation set request
5265
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_DEFAULT#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_DEFAULTValue:
0x8b
Light lightness, color hue, and color saturation default set request
5268
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_RANGE#
#define SL_BTMESH_GENERIC_CLIENT_REQUEST_HSL_RANGEValue:
0x8c
Light color hue and color saturation range set request
5271
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h