Bluetooth Mesh Large Composition Data Server Model#
Bluetooth Mesh Large Composition Data Server Model.
This class provides the commands and messages to interface with the Large Composition Data Server model.
Macros#
#define
sl_btmesh_cmd_lcd_server_init_id 0x01670028
#define
sl_btmesh_cmd_lcd_server_deinit_id 0x02670028
#define
sl_btmesh_rsp_lcd_server_init_id 0x01670028
#define
sl_btmesh_rsp_lcd_server_deinit_id 0x02670028
Function Documentation#
sl_btmesh_lcd_server_init#
sl_status_t sl_btmesh_lcd_server_init ()
Initializes the Large Composition Data Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
21896
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_lcd_server_deinit#
sl_status_t sl_btmesh_lcd_server_deinit ()
Deinitialize the Large Composition Data Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
21906
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h