Bluetooth Mesh Scheduler Client Model#
Bluetooth Mesh Scheduler Client Model.
This class provides commands and messages to interface with the Scheduler Client model. Scheduler models uses multiple fields to define the occurrence of an event and the type of event to be triggered.
For the description of these fields, please see Scheduler Server
Modules#
sl_btmesh_evt_scheduler_client_status
sl_btmesh_evt_scheduler_client_action_status
Functions#
Macros#
Function Documentation#
sl_btmesh_scheduler_client_init#
sl_status_t sl_btmesh_scheduler_client_init (uint16_t elem_index)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index  | 
Initializes the Scheduler Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_client_deinit#
sl_status_t sl_btmesh_scheduler_client_deinit (uint16_t elem_index)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index  | 
Deinitialize the Scheduler Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_scheduler_client_get#
sl_status_t sl_btmesh_scheduler_client_get (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use.  | 
Send a Scheduler Get message to get the Scheduler Register status of a Scheduler Server.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_scheduler_client_get_action#
sl_status_t sl_btmesh_scheduler_client_get_action (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t index)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use.  | 
| uint8_t | [in] | index | Index of the Scheduler Register entry to get  | 
Send a Scheduler Action Get message to get action defined by a Schedule Register state entry.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_scheduler_client_set_action#
sl_status_t sl_btmesh_scheduler_client_set_action (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint8_t index, uint8_t year, uint16_t month, uint8_t day, uint8_t hour, uint8_t minute, uint8_t second, uint8_t day_of_week, uint8_t action, uint32_t transition_time_ms, uint16_t scene_number)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use.  | 
| uint8_t | [in] | flags | Bit 1 (0x02) defines whether response is required, othewise the unacknowledged message is used.  | 
| uint8_t | [in] | index | Index of the Scheduler Register entry to set  | 
| uint8_t | [in] | year | Scheduled year for the action  | 
| uint16_t | [in] | month | Scheduled month for the action  | 
| uint8_t | [in] | day | Scheduled day of the month for the action  | 
| uint8_t | [in] | hour | Scheduled hour for the action  | 
| uint8_t | [in] | minute | Scheduled minute for the action  | 
| uint8_t | [in] | second | Scheduled second for the action  | 
| uint8_t | [in] | day_of_week | Scheduled days of the week for the action  | 
| uint8_t | [in] | action | Action to be performed at the scheduled time  | 
| uint32_t | [in] | transition_time_ms | Transition time for this action  | 
| uint16_t | [in] | scene_number | Scene number to be used for some actions  | 
Send a Scheduler Action Set message to set the given entry of the Scheduler Register state.
For the description of these fields, see Scheduler Server
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events