Bluetooth Mesh Scene Setup Server Model#
Bluetooth Mesh Scene Setup Server Model.
Bluetooth Mesh Scene model Setup Server functionality.
Modules#
sl_btmesh_evt_scene_setup_server_store
sl_btmesh_evt_scene_setup_server_delete
sl_btmesh_evt_scene_setup_server_publish
Functions#
sl_status_t
sl_btmesh_scene_setup_server_init(uint16_t elem_index)
Macros#
#define
sl_btmesh_cmd_scene_setup_server_init_id 0x00510028
#define
sl_btmesh_rsp_scene_setup_server_init_id 0x00510028
Function Documentation#
sl_btmesh_scene_setup_server_init#
sl_status_t sl_btmesh_scene_setup_server_init (uint16_t elem_index)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Index of the element.  | 
Initialize the Scene Setup Server model. Server does not have any internal configurations. The command only activates the model in the mesh stack.
Returns
SL_STATUS_OK if successful. Error code otherwise.