Bluetooth Mesh Stack Provisioner#

Bluetooth Mesh Stack Provisioner.

Bluetooth mesh stack API for the embedded Provisioner

Commands in this class provision nodes in the mesh network and generate security keys for the network.

Initialization:

Provisioning a node:

Key Management

Device Database

These commands are available only if the Provisioner functionality is compiled in the device. Otherwise, a "feature not implemented" error code will be returned for all functions in this class.

Modules#

OOB Capabilities

sl_btmesh_evt_prov_initialized

sl_btmesh_evt_prov_provisioning_suspended

sl_btmesh_evt_prov_capabilities

sl_btmesh_evt_prov_provisioning_failed

sl_btmesh_evt_prov_device_provisioned

sl_btmesh_evt_prov_unprov_beacon

sl_btmesh_evt_prov_oob_pkey_request

sl_btmesh_evt_prov_oob_auth_request

sl_btmesh_evt_prov_oob_display_input

sl_btmesh_evt_prov_ddb_list

sl_btmesh_evt_prov_uri

sl_btmesh_evt_prov_key_refresh_phase_update

sl_btmesh_evt_prov_key_refresh_node_update

sl_btmesh_evt_prov_key_refresh_complete

sl_btmesh_evt_prov_add_ddb_entry_complete

sl_btmesh_evt_prov_delete_ddb_entry_complete

sl_btmesh_evt_prov_initialization_failed

sl_btmesh_evt_prov_provisioning_records_list

sl_btmesh_evt_prov_provisioning_record_data

sl_btmesh_evt_prov_start_sent

Functions#

sl_status_t
sl_status_t
sl_btmesh_prov_create_provisioning_session(uint16_t netkey_index, uuid_128 uuid, uint8_t attention_timer_sec)
sl_status_t
sl_status_t
sl_btmesh_prov_provision_gatt_device(uuid_128 uuid, uint8_t connection)
sl_status_t
sl_btmesh_prov_provision_remote_device(uuid_128 uuid, uint16_t server)
sl_status_t
sl_status_t
sl_btmesh_prov_abort_provisioning(uuid_128 uuid, uint8_t reason)
sl_status_t
sl_btmesh_prov_set_device_address(uuid_128 uuid, uint16_t address)
sl_status_t
sl_btmesh_prov_create_network(uint16_t netkey_index, size_t key_len, const uint8_t *key)
sl_status_t
sl_btmesh_prov_create_appkey(uint16_t netkey_index, uint16_t appkey_index, size_t key_len, const uint8_t *key, size_t max_application_key_size, size_t *application_key_len, uint8_t *application_key)
sl_status_t
sl_btmesh_prov_send_oob_pkey_response(uuid_128 uuid, size_t pkey_len, const uint8_t *pkey)
sl_status_t
sl_btmesh_prov_send_oob_auth_response(uuid_128 uuid, size_t data_len, const uint8_t *data)
sl_status_t
sl_btmesh_prov_set_oob_requirements(uuid_128 uuid, uint8_t public_key, uint8_t auth_methods, uint16_t output_actions, uint16_t input_actions, uint8_t min_size, uint8_t max_size)
sl_status_t
sl_btmesh_prov_start_key_refresh(uint16_t netkey_index, uint8_t num_appkeys, size_t appkey_indices_len, const uint8_t *appkey_indices)
sl_status_t
sl_btmesh_prov_get_key_refresh_exclusion(uint16_t key, uuid_128 uuid, uint8_t *status)
sl_status_t
sl_btmesh_prov_set_key_refresh_exclusion(uint16_t key, uint8_t status, uuid_128 uuid)
sl_status_t
sl_btmesh_prov_set_key_refresh_failure(uint16_t key, uuid_128 uuid)
sl_status_t
sl_btmesh_prov_phase_timeout_get(uint32_t *phase_timeout_s)
sl_status_t
sl_btmesh_prov_phase_timeout_set(uint32_t phase_timeout_s)
sl_status_t
sl_btmesh_prov_get_ddb_entry(uuid_128 uuid, aes_key_128 *device_key, uint16_t *netkey_index, uint16_t *address, uint8_t *elements)
sl_status_t
sl_status_t
sl_btmesh_prov_add_ddb_entry(uuid_128 uuid, aes_key_128 device_key, uint16_t netkey_index, uint16_t address, uint8_t elements)
sl_status_t
sl_status_t
sl_btmesh_prov_initialize_network(uint16_t address, uint32_t ivi)
sl_status_t
sl_btmesh_prov_get_key_refresh_appkey_exclusion(uint16_t netkey_index, uint16_t appkey_index, uuid_128 uuid, uint8_t *status)
sl_status_t
sl_btmesh_prov_set_key_refresh_appkey_exclusion(uint16_t netkey_index, uint16_t appkey_index, uint8_t status, uuid_128 uuid)
sl_status_t
sl_btmesh_prov_update_device_netkey_index(uuid_128 uuid, uint16_t netkey_index)
sl_status_t
sl_btmesh_prov_suspend_key_refresh(uint16_t netkey_index)
sl_status_t
sl_btmesh_prov_resume_key_refresh(uint16_t netkey_index)
sl_status_t
sl_btmesh_prov_get_key_refresh_phase(uint16_t netkey_index, uint8_t *phase)
sl_status_t
sl_btmesh_prov_start_key_refresh_from_phase(uint8_t phase, uint16_t netkey_index, uint8_t num_appkeys, size_t appkey_indices_len, const uint8_t *appkey_indices)
sl_status_t
SL_BGAPI_DEPRECATED sl_status_t
sl_btmesh_prov_test_identity(uint16_t address, uint16_t netkey_index, size_t data_len, const uint8_t *data, uint8_t *match)
sl_status_t
sl_btmesh_prov_get_provisioning_record_data(uuid_128 uuid, uint16_t record)

Macros#

#define
sl_btmesh_cmd_prov_init_id 0x00150028
#define
sl_btmesh_cmd_prov_scan_unprov_beacons_id 0x01150028
#define
sl_btmesh_cmd_prov_create_provisioning_session_id 0x41150028
#define
sl_btmesh_cmd_prov_set_provisioning_suspend_event_id 0x42150028
#define
sl_btmesh_cmd_prov_provision_adv_device_id 0x43150028
#define
sl_btmesh_cmd_prov_provision_gatt_device_id 0x44150028
#define
sl_btmesh_cmd_prov_provision_remote_device_id 0x7f150028
#define
sl_btmesh_cmd_prov_continue_provisioning_id 0x45150028
#define
sl_btmesh_cmd_prov_abort_provisioning_id 0x47150028
#define
sl_btmesh_cmd_prov_set_device_address_id 0x46150028
#define
sl_btmesh_cmd_prov_create_network_id 0x03150028
#define
sl_btmesh_cmd_prov_create_appkey_id 0x07150028
#define
sl_btmesh_cmd_prov_send_oob_pkey_response_id 0x08150028
#define
sl_btmesh_cmd_prov_send_oob_auth_response_id 0x09150028
#define
sl_btmesh_cmd_prov_set_oob_requirements_id 0x0a150028
#define
sl_btmesh_cmd_prov_start_key_refresh_id 0x0b150028
#define
sl_btmesh_cmd_prov_get_key_refresh_exclusion_id 0x0c150028
#define
sl_btmesh_cmd_prov_set_key_refresh_exclusion_id 0x0d150028
#define
sl_btmesh_cmd_prov_set_key_refresh_failure_id 0x12150028
#define
sl_btmesh_cmd_prov_phase_timeout_get_id 0x10150028
#define
sl_btmesh_cmd_prov_phase_timeout_set_id 0x11150028
#define
sl_btmesh_cmd_prov_get_ddb_entry_id 0x16150028
#define
sl_btmesh_cmd_prov_delete_ddb_entry_id 0x17150028
#define
sl_btmesh_cmd_prov_add_ddb_entry_id 0x18150028
#define
sl_btmesh_cmd_prov_list_ddb_entries_id 0x19150028
#define
sl_btmesh_cmd_prov_initialize_network_id 0x37150028
#define
sl_btmesh_cmd_prov_get_key_refresh_appkey_exclusion_id 0x38150028
#define
sl_btmesh_cmd_prov_set_key_refresh_appkey_exclusion_id 0x39150028
#define
sl_btmesh_cmd_prov_stop_scan_unprov_beacons_id 0x3a150028
#define
sl_btmesh_cmd_prov_update_device_netkey_index_id 0x3b150028
#define
sl_btmesh_cmd_prov_suspend_key_refresh_id 0x3c150028
#define
sl_btmesh_cmd_prov_resume_key_refresh_id 0x3d150028
#define
sl_btmesh_cmd_prov_get_key_refresh_phase_id 0x3e150028
#define
sl_btmesh_cmd_prov_start_key_refresh_from_phase_id 0x3f150028
#define
sl_btmesh_cmd_prov_flush_key_refresh_state_id 0x40150028
#define
sl_btmesh_cmd_prov_test_identity_id 0x48150028
#define
sl_btmesh_cmd_prov_get_provisioning_records_list_id 0x1c150028
#define
sl_btmesh_cmd_prov_get_provisioning_record_data_id 0x1d150028
#define
sl_btmesh_cmd_prov_init_provisioning_records_id 0x1e150028
#define
sl_btmesh_rsp_prov_init_id 0x00150028
#define
sl_btmesh_rsp_prov_scan_unprov_beacons_id 0x01150028
#define
sl_btmesh_rsp_prov_create_provisioning_session_id 0x41150028
#define
sl_btmesh_rsp_prov_set_provisioning_suspend_event_id 0x42150028
#define
sl_btmesh_rsp_prov_provision_adv_device_id 0x43150028
#define
sl_btmesh_rsp_prov_provision_gatt_device_id 0x44150028
#define
sl_btmesh_rsp_prov_provision_remote_device_id 0x7f150028
#define
sl_btmesh_rsp_prov_continue_provisioning_id 0x45150028
#define
sl_btmesh_rsp_prov_abort_provisioning_id 0x47150028
#define
sl_btmesh_rsp_prov_set_device_address_id 0x46150028
#define
sl_btmesh_rsp_prov_create_network_id 0x03150028
#define
sl_btmesh_rsp_prov_create_appkey_id 0x07150028
#define
sl_btmesh_rsp_prov_send_oob_pkey_response_id 0x08150028
#define
sl_btmesh_rsp_prov_send_oob_auth_response_id 0x09150028
#define
sl_btmesh_rsp_prov_set_oob_requirements_id 0x0a150028
#define
sl_btmesh_rsp_prov_start_key_refresh_id 0x0b150028
#define
sl_btmesh_rsp_prov_get_key_refresh_exclusion_id 0x0c150028
#define
sl_btmesh_rsp_prov_set_key_refresh_exclusion_id 0x0d150028
#define
sl_btmesh_rsp_prov_set_key_refresh_failure_id 0x12150028
#define
sl_btmesh_rsp_prov_phase_timeout_get_id 0x10150028
#define
sl_btmesh_rsp_prov_phase_timeout_set_id 0x11150028
#define
sl_btmesh_rsp_prov_get_ddb_entry_id 0x16150028
#define
sl_btmesh_rsp_prov_delete_ddb_entry_id 0x17150028
#define
sl_btmesh_rsp_prov_add_ddb_entry_id 0x18150028
#define
sl_btmesh_rsp_prov_list_ddb_entries_id 0x19150028
#define
sl_btmesh_rsp_prov_initialize_network_id 0x37150028
#define
sl_btmesh_rsp_prov_get_key_refresh_appkey_exclusion_id 0x38150028
#define
sl_btmesh_rsp_prov_set_key_refresh_appkey_exclusion_id 0x39150028
#define
sl_btmesh_rsp_prov_stop_scan_unprov_beacons_id 0x3a150028
#define
sl_btmesh_rsp_prov_update_device_netkey_index_id 0x3b150028
#define
sl_btmesh_rsp_prov_suspend_key_refresh_id 0x3c150028
#define
sl_btmesh_rsp_prov_resume_key_refresh_id 0x3d150028
#define
sl_btmesh_rsp_prov_get_key_refresh_phase_id 0x3e150028
#define
sl_btmesh_rsp_prov_start_key_refresh_from_phase_id 0x3f150028
#define
sl_btmesh_rsp_prov_flush_key_refresh_state_id 0x40150028
#define
sl_btmesh_rsp_prov_test_identity_id 0x48150028
#define
sl_btmesh_rsp_prov_get_provisioning_records_list_id 0x1c150028
#define
sl_btmesh_rsp_prov_get_provisioning_record_data_id 0x1d150028
#define
sl_btmesh_rsp_prov_init_provisioning_records_id 0x1e150028

Function Documentation#

sl_btmesh_prov_init#

sl_status_t sl_btmesh_prov_init ()

Initialize the Bluetooth mesh stack in the Provisioner role. Note that the result code of this command only indicates that the request to initialize has been accepted for processing. When initialization is completed successfully, a sl_btmesh_evt_prov_initialized will be generated. On failed initialization a sl_btmesh_evt_prov_initialization_failed event will be generated. Note that the application must wait for an event to be generated before executing further BGAPI commands.

This command must be issued before any other Bluetooth mesh stack commands. Note that the Bluetooth mesh stack can be initialized either in the Provisioner or the Node role, but not both.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2817 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_scan_unprov_beacons#

sl_status_t sl_btmesh_prov_scan_unprov_beacons ()

Start scanning for unprovisioned device beacons.

Unprovisioned devices send out beacons containing their UUID. An sl_btmesh_evt_prov_unprov_beacon will be generated for each beacon seen. Once the UUID of a device is known, the Provisioner may start provisioning the device with the sl_btmesh_prov_create_provisioning_session command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2835 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_create_provisioning_session#

sl_status_t sl_btmesh_prov_create_provisioning_session (uint16_t netkey_index, uuid_128 uuid, uint8_t attention_timer_sec)
Parameters
[in]netkey_index

Index of the initial network key, which is sent to the device during provisioning

[in]uuid

UUID of the device

[in]attention_timer_sec

Attention timer value, in seconds, which indicates the time that the provisioned device should attract human attention

Initialize the provisioning session. After this command, it is possible to set the provisioning parameter with the following command:

After all optional parameters have been set, the provisioning process is triggered by one of the following commands:

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2863 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_provisioning_suspend_event#

sl_status_t sl_btmesh_prov_set_provisioning_suspend_event (uint8_t status)
Parameters
[in]status

Controls when provisioning is suspended and sl_btmesh_evt_prov_provisioning_suspended event is created. The value is a bitmap so multiple possibilities can be set.

  • Bit 0 set provisioning will be suspended when Capabilities PDU is received from the unprovisioned device

  • Bit 1 set provisioning will be suspended when the provisioning session is opened

If no bits are set (value is zero) provisioning will not be suspended. This is the default.

Set whether the provisioning can be suspended at a specified point while it is occurring. Currently, this can happen after reception on provisioning capabilities message or when the provisioning link is opened.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2893 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_provision_adv_device#

sl_status_t sl_btmesh_prov_provision_adv_device (uuid_128 uuid)
Parameters
[in]uuid

UUID of the device

Provision device over PB-ADV

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2908 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_provision_gatt_device#

sl_status_t sl_btmesh_prov_provision_gatt_device (uuid_128 uuid, uint8_t connection)
Parameters
[in]uuid

UUID of the device

[in]connection

Connection handle

Provision device over PB-GATT

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2925 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_provision_remote_device#

sl_status_t sl_btmesh_prov_provision_remote_device (uuid_128 uuid, uint16_t server)
Parameters
[in]uuid

UUID of the device

[in]server

Address of the remote provisioning server

Provision device over remote provisioning server connection

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2943 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_continue_provisioning#

sl_status_t sl_btmesh_prov_continue_provisioning (uuid_128 uuid)
Parameters
[in]uuid

UUID of the device being provisioned

Continue provisioning after the suspension indicated by sl_btmesh_evt_prov_provisioning_suspended.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2959 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_abort_provisioning#

sl_status_t sl_btmesh_prov_abort_provisioning (uuid_128 uuid, uint8_t reason)
Parameters
[in]uuid

UUID of the device being provisioned

[in]reason

Reason for aborting. Values are as follows:

  • 1: Invalid PDU

  • 2: Invalid PDU format

  • 3: Unexpected PDU

  • 4: Confirmation failed

  • 5: Out of resources

  • 6: Decryption failed

  • 7: Unexpected error

  • 8: Unable to assign address

Abort provisioning. This command is typically used after the suspension indicated by sl_btmesh_evt_prov_provisioning_suspended.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2983 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_device_address#

sl_status_t sl_btmesh_prov_set_device_address (uuid_128 uuid, uint16_t address)
Parameters
[in]uuid

UUID of the device being provisioned

[in]address

Unicast address to be assigned for the primary element of the node.

Set the address for the device after the provisioning has been suspended, as indicated by sl_btmesh_evt_prov_provisioning_suspended event.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3000 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_create_network#

sl_status_t sl_btmesh_prov_create_network (uint16_t netkey_index, size_t key_len, const uint8_t * key)
Parameters
[in]netkey_index

Index to use for network key. Allowed values are from 0x000 to 0xfff.

[in]key_len

Length of data in key

[in]key

Key value to use. Set to zero-length array to generate a random key.

Create a new network key on the Provisioner.

The created key can be deployed on a node using the sl_btmesh_config_client_add_netkey command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3018 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_create_appkey#

sl_status_t sl_btmesh_prov_create_appkey (uint16_t netkey_index, uint16_t appkey_index, size_t key_len, const uint8_t * key, size_t max_application_key_size, size_t * application_key_len, uint8_t * application_key)
Parameters
[in]netkey_index

Index of the network key to which the application key will be bound

[in]appkey_index

Index to use for application key. Allowed values are from 0x000 to 0xfff.

[in]key_len

Length of data in key

[in]key

Key value to use; set to zero-length array to generate random key.

[in]max_application_key_size

Size of output buffer passed in application_key

[out]application_key_len

On return, set to the length of output data written to application_key

[out]application_key

New application key. Ignore it if the result was non-zero.

Create a new application key on the Provisioner.

An application key is always bound to a network key. In other words, the application key is only valid in the context of a particular network key. The selected network key must exist on the Provisioner (see sl_btmesh_prov_create_network command).

The created application key can be deployed on a node using the sl_btmesh_config_client_add_appkey command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3051 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_send_oob_pkey_response#

sl_status_t sl_btmesh_prov_send_oob_pkey_response (uuid_128 uuid, size_t pkey_len, const uint8_t * pkey)
Parameters
[in]uuid

UUID of the Device

[in]pkey_len

Length of data in pkey

[in]pkey

Public Key read out-of-band

Respond to the prov_oob_pkey_request.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3070 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_send_oob_auth_response#

sl_status_t sl_btmesh_prov_send_oob_auth_response (uuid_128 uuid, size_t data_len, const uint8_t * data)
Parameters
[in]uuid

UUID of the Device

[in]data_len

Length of data in data

[in]data

Raw 16-byte or 32-byte array containing the static or output authentication data. The length of the data depends on the chosen provisioning algorithm; see sl_btmesh_evt_prov_start_sent event for details on how to determine which provisioning algorithm was chosen.

Note that the raw data given to the stack must be encoded in the manner described in the Mesh Protocol 1.1 specifcation Section 5.4.2.4. Whether the output data should be treated as Numeric or Alphanumeric depends on the selected output action. The data type for Static OOB authentication data is Binary.

Respond to the prov_oob_auth_request.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3096 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_oob_requirements#

sl_status_t sl_btmesh_prov_set_oob_requirements (uuid_128 uuid, uint8_t public_key, uint8_t auth_methods, uint16_t output_actions, uint16_t input_actions, uint8_t min_size, uint8_t max_size)
Parameters
[in]uuid

UUID of the Device being provisioned

[in]public_key

The public key. Set to zero if the provisioning does not use OOB public Key.

[in]auth_methods

Enum sl_btmesh_node_auth_method_flag_t. Allowed OOB authentication methods The value is a bitmap so that multiple methods can be supported.

[in]output_actions

Enum sl_btmesh_node_oob_output_action_flag_t. Allowed OOB Output Action types

[in]input_actions

Enum sl_btmesh_node_oob_input_action_flag_t. Allowed OOB Input Action types

[in]min_size

Minimum input/output OOB size. Values range from 0 (input/output OOB not used) to 8.

[in]max_size

Maximum input/output OOB size. Must be larger than or equal to the minimum size. Values range from 0 (input/output OOB not used) to 8.

Set the OOB requirements for a device being provisioned. This command can be issued after sl_btmesh_prov_create_provisioning_session.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3124 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_start_key_refresh#

sl_status_t sl_btmesh_prov_start_key_refresh (uint16_t netkey_index, uint8_t num_appkeys, size_t appkey_indices_len, const uint8_t * appkey_indices)
Parameters
[in]netkey_index

Index of the network key to update

[in]num_appkeys

Number of application keys to update; may be zero.

[in]appkey_indices_len

Length of data in appkey_indices

[in]appkey_indices

Indices of the application keys to update, represented as little endian two byte sequences. The array must contain num_appkeys indices and therefore 2*num_appkeys bytes total.

Start a key refresh procedure in the network.

A key refresh procedure updates a network key and, optionally, application keys associated with it in all nodes of the network except for excluded nodes. After the refresh procedure is complete, the old keys will be discarded. Therefore, the excluded nodes, which did not receive new keys will be shut out of the network at the completion of the procedure.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3157 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_key_refresh_exclusion#

sl_status_t sl_btmesh_prov_get_key_refresh_exclusion (uint16_t key, uuid_128 uuid, uint8_t * status)
Parameters
[in]key

Network key index

[in]uuid

UUID of the Device

[out]status

Non-zero for excluded node

Check the key refresh exclusion status of a node. Excluded nodes do not participate in the key refresh procedure and can therefore be shut out of the network.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3175 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_key_refresh_exclusion#

sl_status_t sl_btmesh_prov_set_key_refresh_exclusion (uint16_t key, uint8_t status, uuid_128 uuid)
Parameters
[in]key

Network key index

[in]status

Non-zero for excluded node

[in]uuid

UUID of the Device

Set the key refresh exclusion status of a node. Excluded nodes do not participate in the key refresh procedure and can therefore be shut out of the network.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3192 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_key_refresh_failure#

sl_status_t sl_btmesh_prov_set_key_refresh_failure (uint16_t key, uuid_128 uuid)
Parameters
[in]key

Network key index

[in]uuid

UUID of the Device

Mark the node as failed for the keyrefresh. This function should be called if the provisioner knows that the node has become unresponsive for some external reason (such as factory reset performed by the end user), and will not respond to key refresh messages even after a long delay. Note that if a node drops out of the key refresh procedure, it will not be possible to communicate with the node using the key that was refreshed during the key refresh procedure.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3212 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_phase_timeout_get#

sl_status_t sl_btmesh_prov_phase_timeout_get (uint32_t * phase_timeout_s)
Parameters
[out]phase_timeout_s

Value to get in seconds

Get the phase_timeout_s parameter that will be used for the start key refresh command. A node fails the key refresh procedure phase, if it doesnt reply to the provisioner during the timeout.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3225 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_phase_timeout_set#

sl_status_t sl_btmesh_prov_phase_timeout_set (uint32_t phase_timeout_s)
Parameters
[in]phase_timeout_s

Value to be set in seconds

Set the phase_timeout_s parameter that will be used for the start key refresh command. A node fails the key refresh procedure phase, if it doesnt reply to the provisioner during the timeout. Maximum allowed value is 345600 sec (4days).

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3239 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_ddb_entry#

sl_status_t sl_btmesh_prov_get_ddb_entry (uuid_128 uuid, aes_key_128 * device_key, uint16_t * netkey_index, uint16_t * address, uint8_t * elements)
Parameters
[in]uuid

UUID of the Device to retrieve

[out]device_key

Device Key

[out]netkey_index

Index of the network key with which the node was initially provisioned. Used for network-level encryption of Configuration Client messages.

[out]address

Unicast address of the primary element of the node

[out]elements

Number of elements in the node

Get a Provisioner device database entry with a matching UUID.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3256 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_delete_ddb_entry#

sl_status_t sl_btmesh_prov_delete_ddb_entry (uuid_128 uuid)
Parameters
[in]uuid

UUID of the node to delete

Delete the node information from the Provisioner database. Note that a successful result from this command only means the command has been accepted for processing. The status of the actual operation will be returned in the following event; application should not make new BGAPI requests until the event is received. Note also that this should be followed by a sl_btmesh_prov_start_key_refresh updating the keys of the remaining nodes to make sure the deleted node is shut off from the network.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3280 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_add_ddb_entry#

sl_status_t sl_btmesh_prov_add_ddb_entry (uuid_128 uuid, aes_key_128 device_key, uint16_t netkey_index, uint16_t address, uint8_t elements)
Parameters
[in]uuid

UUID of the node to add

[in]device_key

Device key value for the node

[in]netkey_index

Index of the network key the node will be used for configuration

[in]address

Unicast address to allocate for the node's primary element

[in]elements

Number of elements the device has

Add a new node entry to the Provisioner's device database. Note that a successful result from this command only means the command has been accepted for processing. The status of the actual operation will be returned in the following event; application should not make new BGAPI requests until the event is received. Note also that the device key, primary element address, and network key need to be deployed to the node being added to ensure it's configurable. See sl_btmesh_node_set_provisioning_data command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3305 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_list_ddb_entries#

sl_status_t sl_btmesh_prov_list_ddb_entries (uint16_t * count)
Parameters
[out]count

Number of events that will follow

List nodes known by this Provisioner. A number of sl_btmesh_evt_prov_ddb_list events will be generated.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3324 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_initialize_network#

sl_status_t sl_btmesh_prov_initialize_network (uint16_t address, uint32_t ivi)
Parameters
[in]address

Address to assign for provisioner.

[in]ivi

IV index of the network.

Initialize the mesh network and assign the provisioner address and IV index for the network. If this command is not invoked prior to invoking sl_btmesh_prov_create_network, the network will be initialized with default address and IV index.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3339 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_key_refresh_appkey_exclusion#

sl_status_t sl_btmesh_prov_get_key_refresh_appkey_exclusion (uint16_t netkey_index, uint16_t appkey_index, uuid_128 uuid, uint8_t * status)
Parameters
[in]netkey_index

Network key index

[in]appkey_index

Application key index

[in]uuid

UUID of the Device

[out]status

Non-zero for excluded node

Check the application key refresh exclusion status of a node. Nodes which are excluded for a given application key do not receive updates for that particular application key, but do participate in the key refresh procedure as a whole. This enables the Provisioner to set up and update restricted sets of application keys across nodes.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3357 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_set_key_refresh_appkey_exclusion#

sl_status_t sl_btmesh_prov_set_key_refresh_appkey_exclusion (uint16_t netkey_index, uint16_t appkey_index, uint8_t status, uuid_128 uuid)
Parameters
[in]netkey_index

Network key index

[in]appkey_index

Application key index

[in]status

Non-zero for excluded node

[in]uuid

UUID of the device

Set the application key refresh exclusion status of a node. Nodes which are excluded for a given application key do not receive updates for that particular application key, but do participate in the key refresh procedure as a whole. This enables the Provisioner to set up and update restricted sets of application keys across nodes.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3378 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_stop_scan_unprov_beacons#

sl_status_t sl_btmesh_prov_stop_scan_unprov_beacons ()

Stop scanning for unprovisioned device beacons.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3391 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_update_device_netkey_index#

sl_status_t sl_btmesh_prov_update_device_netkey_index (uuid_128 uuid, uint16_t netkey_index)
Parameters
[in]uuid

UUID of the node

[in]netkey_index

Index of the network key used in configuring the node.

Update a node's entry in the Provisioner's device database by setting a new value to the netkey_index field. The netkey_index field is used to determine the network key to use when encrypting and decrypting configuration model messages to and from the node.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3407 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_suspend_key_refresh#

sl_status_t sl_btmesh_prov_suspend_key_refresh (uint16_t netkey_index)
Parameters
[in]netkey_index

Index of the network key identifying an ongoing key refresh procedure

Suspend an ongoing key refresh procedure.

Suspending a key refresh procedure means no further requests for updating keys or setting key refresh phase will be sent to the network by the Provisioner until the key refresh procedure is resumed.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3424 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_resume_key_refresh#

sl_status_t sl_btmesh_prov_resume_key_refresh (uint16_t netkey_index)
Parameters
[in]netkey_index

Index of the network key identifying a suspended key refresh procedure

Resume a suspended key refresh procedure.

By resuming a suspended key refresh procedure, the Provisioner will again start to send requests for updating keys or setting key refresh phase to the network.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3440 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_key_refresh_phase#

sl_status_t sl_btmesh_prov_get_key_refresh_phase (uint16_t netkey_index, uint8_t * phase)
Parameters
[in]netkey_index

Index of the network key identifying an ongoing key refresh procedure

[out]phase

The current key refresh phase. Values are as follows:

  • 0: Normal operation (no ongoing key refresh)

  • 1: First phase of key refresh procedure (key deployment)

  • 2: Second phase of key refresh procedure (new key activation)

  • 3: Third phase of key refresh procedure (old key deletion)

Get the key refresh phase of an ongoing key refresh procedure.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3457 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_start_key_refresh_from_phase#

sl_status_t sl_btmesh_prov_start_key_refresh_from_phase (uint8_t phase, uint16_t netkey_index, uint8_t num_appkeys, size_t appkey_indices_len, const uint8_t * appkey_indices)
Parameters
[in]phase

Current key refresh phase

[in]netkey_index

Index of the network key identifying a key refresh procedure

[in]num_appkeys

Number of application keys to update; may be zero.

[in]appkey_indices_len

Length of data in appkey_indices

[in]appkey_indices

Indices of the application keys to update, represented as little endian two byte sequences. The array must contain num_appkeys indices and therefore 2*num_appkeys bytes total.

Start a key refresh procedure from a non-default phase. Before calling this function, keys to be used in the key refresh procedure should have been specified by calling sl_btmesh_test_prov_prepare_key_refresh command.

Note that this command should not normally be used. It is intended only for resuming an interrupted key refresh procedure on a backup Provisioner when the original Provisioner, that started the key refresh procedure, is no longer available to complete the procedure.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3488 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_flush_key_refresh_state#

sl_status_t sl_btmesh_prov_flush_key_refresh_state (uint16_t netkey_index)
Parameters
[in]netkey_index

Index of the network key identifying a key refresh procedure

Clear the key refresh state stored in persistent storage.

Note that this command should not normally be used. It is intended only for clearing stored key refresh state when a key refresh procedure has been suspended and will not be resumed, either because the network key has been deleted from all nodes or the responsibility for completing the key refresh has been moved to another Provisioner.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3510 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_test_identity#

SL_BGAPI_DEPRECATED sl_status_t sl_btmesh_prov_test_identity (uint16_t address, uint16_t netkey_index, size_t data_len, const uint8_t * data, uint8_t * match)
Parameters
[in]address

Mesh address of the node

[in]netkey_index

Network key index of the node.

[in]data_len

Length of data in data

[in]data

Contents of the identity beacon.

[out]match

- 0: Identity record did not match

  • 1: Identity record match

Test if data in the identity beacon matches the mesh device and network. This is a deprecated function. Please use sl_btmesh_node_test_identity

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3527 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_provisioning_records_list#

sl_status_t sl_btmesh_prov_get_provisioning_records_list (uuid_128 uuid)
Parameters
[in]uuid

UUID of the Device being provisioned

Get the list of provisioning records on the device. This command can be issued when provisioning is suspended after the provisioning session has been opened, but no earlier or later. The list of provisioning records on the device will be delivered with the sl_btmesh_evt_prov_provisioning_records_list event.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3549 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_get_provisioning_record_data#

sl_status_t sl_btmesh_prov_get_provisioning_record_data (uuid_128 uuid, uint16_t record)
Parameters
[in]uuid

UUID of the Device being provisioned

[in]record

Provisioning record ID

Get provisioning record data from the device. This command can be issued when provisioning is suspended after the provisioning session has been opened, but no earlier or later. The provisioning record data will be delivered with the sl_btmesh_evt_prov_provisioning_record_data event.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 3567 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_prov_init_provisioning_records#

sl_status_t sl_btmesh_prov_init_provisioning_records ()

Initialize provisioning record retrieval functionality on the Provisioner. This must be called before trying to retrieve provisioning records list or individual record data.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 3580 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h