Bluetooth Mesh Sensor Setup Server Model#
Bluetooth Mesh Sensor Setup Server Model.
This class provides the commands and messages to interface with the Sensor Setup Server model. Elements containing sensor model must have a setup server model attached. Therefore, it is initialized/deinitialized internally together with the server model.
Modules#
sl_btmesh_evt_sensor_setup_server_get_cadence_request
sl_btmesh_evt_sensor_setup_server_set_cadence_request
sl_btmesh_evt_sensor_setup_server_get_settings_request
sl_btmesh_evt_sensor_setup_server_get_setting_request
sl_btmesh_evt_sensor_setup_server_set_setting_request
sl_btmesh_evt_sensor_setup_server_publish
Functions#
Macros#
Function Documentation#
sl_btmesh_sensor_setup_server_send_cadence_status#
sl_status_t sl_btmesh_sensor_setup_server_send_cadence_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t params_len, const uint8_t * params)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | client_address | Destination client address The address 0x0000 can be used to publish the message according model configuration instead of a direct reply.  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use  | 
| uint8_t | [in] | flags | No flags defined currently  | 
| uint16_t | [in] | property_id | Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.  | 
| size_t | [in] | params_len | Length of data in   | 
| const uint8_t * | [in] | params | Optional byte array containing the serialized Sensor Cadence state, excluding the property ID. If not empty, the state consists of the following fields: 
  | 
Reply to a Get/Set Cadence client request with a Cadence Status message. Only Cadence Set (acknowledged) must be answered by sending the status message to the client. In addition, configuration changes must be published according to model publishing configuration.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_sensor_setup_server_send_settings_status#
sl_status_t sl_btmesh_sensor_setup_server_send_settings_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, size_t setting_ids_len, const uint8_t * setting_ids)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | client_address | Destination client model address  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use  | 
| uint8_t | [in] | flags | No flags defined currently  | 
| uint16_t | [in] | property_id | Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.  | 
| size_t | [in] | setting_ids_len | Length of data in   | 
| const uint8_t * | [in] | setting_ids | Array of 16-bit Setting Property IDs of the settings the given sensor has  | 
Reply to a Get Settings client request with a Settings Status message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_sensor_setup_server_send_setting_status#
sl_status_t sl_btmesh_sensor_setup_server_send_setting_status (uint16_t client_address, uint16_t elem_index, uint16_t appkey_index, uint8_t flags, uint16_t property_id, uint16_t setting_id, size_t raw_value_len, const uint8_t * raw_value)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | client_address | Destination client model address  | 
| uint16_t | [in] | elem_index | Client model element index  | 
| uint16_t | [in] | appkey_index | The application key index to use  | 
| uint8_t | [in] | flags | No flags defined currently  | 
| uint16_t | [in] | property_id | Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.  | 
| uint16_t | [in] | setting_id | Sensor Setting Property ID field identifying the device property of a setting. Range: 0x0001 - 0xffff, 0x0000 is prohibited.  | 
| size_t | [in] | raw_value_len | Length of data in   | 
| const uint8_t * | [in] | raw_value | Sensor Setting raw value. Size and representation depends on the type defined by the Sensor Setting Property ID.  | 
Reply to a Get/Set Setting client request with a Setting Status message. Only Set Setting (acknowledged) request must be answered by sending a reply to the unicast address of the sender. In addition, configuration changes must be published if model publishing is set up.
Returns
SL_STATUS_OK if successful. Error code otherwise.