sl_btmesh_evt_config_client_request_modified#

Pending request parameters have been updated.

The application may call sl_btmesh_config_client_get_request_status to retrieve the current status of the request. This event is generated when the timeout of a request is extended because the request is acknowledged by a Friend node on behalf of the LPN, which is the destination of the request.

Modules#

sl_btmesh_evt_config_client_request_modified_s

Macros#

#define
sl_btmesh_evt_config_client_request_modified_id 0x002700a8

Identifier of the request_modified event.

Typedef Documentation#

sl_btmesh_evt_config_client_request_modified_t#

typedef struct sl_btmesh_evt_config_client_request_modified_s sl_btmesh_evt_config_client_request_modified_t