Data structure of the fw_status event.

Public Attributes#

uint16_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::server_address

Unicast address of the server


status#

uint8_t sl_btmesh_evt_fw_dist_client_fw_status_s::status

Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned


num_entries#

uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::num_entries

Number of images stored on the Distributor


index#

uint16_t sl_btmesh_evt_fw_dist_client_fw_status_s::index

Index of the queried firmware on the server. 0xffff if not found.


fwid#

uint8array sl_btmesh_evt_fw_dist_client_fw_status_s::fwid

FWID of the firmware that was queried. Empty if get_by_index was used and no such index exists.