Data structure of the receivers_list_end event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::server_address

Unicast address of the server


start_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::start_index

Starting index


num_reported#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::num_reported

Number of entries reported


nodes_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::nodes_list_size

Number of entries currently in the node list