Data structure of the receivers_list event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::server_address
Unicast address of the server
nodes_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::nodes_list_size
Number of entries currently in the node list
phase#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::phase
Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Phase of the Update Server
update_status#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::update_status
Last Update Status message received from the Update Server
transfer_status#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::transfer_status
Last Transfer Status message received from the BLOB Transfer Server
progress#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::progress
0-100, percentage of BLOB Transfer octets delivered and confirmed
fw_index#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::fw_index
Index of the firmware being updated