Data structure of the node_failed event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_node_failed_s::elem_index

Server model element index


address#

uint16_t sl_btmesh_evt_fw_dist_server_node_failed_s::address

Address of the Update Server


update_phase#

uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::update_phase

Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Update Phase of the Update Server. 0xa if not known yet.


update_status#

uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::update_status

Enum sl_btmesh_fw_update_server_update_status_t. Last Update Status message received from the Update Server


mbt_status#

uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::mbt_status

Last status code received from the MBT Server. 0xa if not known yet.


progress#

uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::progress

0-100, percentage of BLOB Transfer octets delivered and confirmed


fw_index#

uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::fw_index

Index of the firmware being updated