Data structure of the metadata_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_update_client_metadata_status_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_fw_update_client_metadata_status_s::server_address
Unicast address of the server
status#
uint8_t sl_btmesh_evt_fw_update_client_metadata_status_s::status
Enum sl_btmesh_fw_update_server_update_status_t. Status code returned
additional_information#
uint8_t sl_btmesh_evt_fw_update_client_metadata_status_s::additional_information
Enum sl_btmesh_fw_update_client_additional_info_t. Additional information about what will happen to the node after the update is applied. 0 = no changes to DCD; 1 = DCD will change but Composition Data Refresh is not supported; 2 = DCD change and Composition Data Refresh is supported; 3 = node will become unprovisioned.
fw_index#
uint8_t sl_btmesh_evt_fw_update_client_metadata_status_s::fw_index
Index of the firmware that was checked against the metadata.