Data structure of the server_status_attention event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_health_client_server_status_attention_s::client_address

Destination address the message was sent to


elem_index#

uint16_t sl_btmesh_evt_health_client_server_status_attention_s::elem_index

Client model element index. Identifies the client model which received the status message.


server_address#

uint16_t sl_btmesh_evt_health_client_server_status_attention_s::server_address

Address of the Server model which sent the message


result#

uint16_t sl_btmesh_evt_health_client_server_status_attention_s::result

Response status. If an error occurs (e.g., request timeout), ignore the parameters other than element index, client address, and server address.


attention_sec#

uint8_t sl_btmesh_evt_health_client_server_status_attention_s::attention_sec

Current attention timer value in seconds