Data structure of the light_onoff_status event.

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::destination_address

Address of the client or the group address to which it was published.


elem_index#

uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::elem_index

Index of the element for which received the status.


server_address#

uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::server_address

Device which sent the status.


appkey_index#

uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::appkey_index

Appkey used by server_address.


present_light_onoff#

uint8_t sl_btmesh_evt_lc_client_light_onoff_status_s::present_light_onoff

Present value of the Light OnOff state


target_light_onoff#

uint8_t sl_btmesh_evt_lc_client_light_onoff_status_s::target_light_onoff

Target value of the Light OnOff state


remaining_time_ms#

uint32_t sl_btmesh_evt_lc_client_light_onoff_status_s::remaining_time_ms

Time (in milliseconds) remaining in transition