Data structure of the om_updated event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_server_om_updated_s::destination_address

Message destination address if triggered by a message, 0 otherwise.


elem_index#

uint16_t sl_btmesh_evt_lc_server_om_updated_s::elem_index

Index of the element where the update happened


client_address#

uint16_t sl_btmesh_evt_lc_server_om_updated_s::client_address

Message source address if triggered by a message, 0 otherwise.


appkey_index#

uint16_t sl_btmesh_evt_lc_server_om_updated_s::appkey_index

Message appkey index if triggered by a message, 0xFFFF otherwise.


om_value#

uint8_t sl_btmesh_evt_lc_server_om_updated_s::om_value

The value the LC Occupancy Mode state is being set to.