Data structure of the key_updated event.
Public Attribute Documentation#
type#
uint8_t sl_btmesh_evt_node_key_updated_s::type
Type of the updated key. Values are as follows:
0x00: Network key
0x01: Application key
netkey_index#
uint16_t sl_btmesh_evt_node_key_updated_s::netkey_index
Network key index to which the application key is bound. Ignore this value if the event is for network key updates.