Data structure of the private_gatt_proxy_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
handle#
uint32_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::handle
Request handle
value#
uint8_t sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status_s::value
On-Demand Private GATT proxy value of the node. Valid values are:
0: Advertising with Private Network Identity type cannot be enabled on demand
1-255: Advertising interval for Private Network Identity in seconds