Data structure of the scan_capabilities event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::result
SL_STATUS_OK if successful. Error code otherwise.
max_items#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::max_items
The maximum number of UUIDs that can be reported during scanning.
active#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::active
Indication if active scan is supported.