Data structure of the scan_report event.

Public Attributes#

uint16_t
int8_t
uint16_t
uint32_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::server

Server address.


rssi#

int8_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::rssi

measured signal stength in dBm.


uuid#

uuid_128 sl_btmesh_evt_remote_provisioning_client_scan_report_s::uuid

UUID of the unprovisioned device found


oob#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::oob

OOB information.


uri#

uint32_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::uri

Hash of the out-of-band URI, which is received in a separate event . If the URI bit (bit 1) is not set in the OOB capabilities bitfield, this field is ignored.