Data structure of the scan_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


server#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::server

Server address.


status#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::status

Enum sl_btmesh_remote_provisioning_server_status_t. server status.


state#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::state

Enum sl_btmesh_remote_provisioning_server_scan_state_t. Scan state.


max_reports#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::max_reports

Maximum number of scanned items to be reported.


timeout_sec#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::timeout_sec

Maximum available time for time left until the end of the Remote Provisioning Scan procedure.