Data structure of the action_status event.
Public Attributes#
uint16_t
uint16_t
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint32_t
uint16_t
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::client_address
Destination client model address
elem_index#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::server_address
Source server model address
appkey_index#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::appkey_index
The application key index to use.
day#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day
Scheduled day of the month for the action
minute#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::minute
Scheduled minute for the action
second#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::second
Scheduled second for the action
day_of_week#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day_of_week
Scheduled days of the week for the action
action#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::action
Action to be performed at the scheduled time
transition_time_ms#
uint32_t sl_btmesh_evt_scheduler_client_action_status_s::transition_time_ms
Transition time for this action
scene_number#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::scene_number
Scene number to be used for some actions