Data structure of the cadence_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_sensor_client_cadence_status_s::client_address
Destination client model address
elem_index#
uint16_t sl_btmesh_evt_sensor_client_cadence_status_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_sensor_client_cadence_status_s::server_address
Source server model address
appkey_index#
uint16_t sl_btmesh_evt_sensor_client_cadence_status_s::appkey_index
The application key index to use.
property_id#
uint16_t sl_btmesh_evt_sensor_client_cadence_status_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.
params#
uint8array sl_btmesh_evt_sensor_client_cadence_status_s::params
Optional byte array containing serialized fields of Sensor Cadence state, excluding the property ID
Fast Cadence Period Divisor, 7 bits
Status Trigger type, 1 bit (0 = discrete value, 1 = percentage)
Status Trigger Delta Down, variable length
Status Trigger Delta Up, variable length
Status Min Interval, 8 bits, representing a power of 2 milliseconds. Valid range is 0-26
Fast Cadence Low, variable length, lower bound for the fast cadence range
Low Cadence Low, variable length, higher bound for the fast cadence range