Data structure of the settings_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_sensor_client_settings_status_s::client_address
Destination client model address
elem_index#
uint16_t sl_btmesh_evt_sensor_client_settings_status_s::elem_index
Client model element index
server_address#
uint16_t sl_btmesh_evt_sensor_client_settings_status_s::server_address
Source server model address
appkey_index#
uint16_t sl_btmesh_evt_sensor_client_settings_status_s::appkey_index
The application key index to use
property_id#
uint16_t sl_btmesh_evt_sensor_client_settings_status_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.
setting_ids#
uint8array sl_btmesh_evt_sensor_client_settings_status_s::setting_ids
Array of 16-bit Setting Property IDs of the settings the given sensor has