Data structure of the get_cadence_request event.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::server_address
Address the request was directed to, either the server's unicast address or a group address the server subscribes to
elem_index#
uint16_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::elem_index
Setup Server model element index
client_address#
uint16_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::client_address
Requesting client model's address
appkey_index#
uint16_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::appkey_index
The application key index to use
flags#
uint8_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::flags
No flags defined currently
property_id#
uint16_t sl_btmesh_evt_sensor_setup_server_get_cadence_request_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.