Data structure of the publish event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_sensor_setup_server_publish_s::elem_index
Client model element index
period_ms#
uint32_t sl_btmesh_evt_sensor_setup_server_publish_s::period_ms
The current publishing period that can be used to estimate the next tick, e.g., when the state should be reported at higher frequency.