Data structure of the model_status event.
Public Attribute Documentation#
status#
uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::status
Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.
elem_index#
uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::elem_index
Element index of model to configure.
vendor_id#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::vendor_id
Vendor ID of model to configure.
model_id#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::model_id
Model ID of model to configure.
value#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::value
Extended packet size to set, currently 1 to use extended 0 to not