Data structure of the items_status event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

src#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::src

Server address


dst#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::dst

Client address


appkey_index#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::appkey_index

App key index


range_start#

uint16_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_start

15 least significant bits of the starting unicast address


length_present#

uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::length_present

Indicates the presence or absence of the RangeLength field


range_length#

uint8_t sl_btmesh_evt_solicitation_config_client_items_status_s::range_length

If present, containsNumber of addresses in the range (0x02 – 0xFF), otherwise 0