Data structure of the time_zone_status event.

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_time_client_time_zone_status_s::client_address

Client address


elem_index#

uint16_t sl_btmesh_evt_time_client_time_zone_status_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_time_client_time_zone_status_s::server_address

Unicast address of the server


appkey_index#

uint16_t sl_btmesh_evt_time_client_time_zone_status_s::appkey_index

App key index.


time_zone_offset_current#

int16_t sl_btmesh_evt_time_client_time_zone_status_s::time_zone_offset_current

Current local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.


time_zone_offset_new#

int16_t sl_btmesh_evt_time_client_time_zone_status_s::time_zone_offset_new

Upcoming local time zone offset


tai_of_zone_change#

uint64_t sl_btmesh_evt_time_client_time_zone_status_s::tai_of_zone_change

TAI seconds time of the upcoming Time Zone offset change