Data structure of the time_zone_offset_updated event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::elem_index
Server model element index
time_zone_offset_current#
int16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::time_zone_offset_current
Current local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.
time_zone_offset_new#
int16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::time_zone_offset_new
Upcoming local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.
tai_of_zone_change#
uint64_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::tai_of_zone_change
Absolute TAI time when the Time Zone Offset will change from Current to New