Data structure of the resume_req event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::elem_index

Server model element index


Definition at line 17811 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::client_address

Address of the Distribution Client


Definition at line 17812 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

group_address#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::group_address

Group address to use for the distribution


Definition at line 17813 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

app_index#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::app_index

Appkey index to use for the distribution


Definition at line 17814 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ttl#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::ttl

TTL to use for the distribution


Definition at line 17815 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

update_policy#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::update_policy

Update Policy to use for the distribution


Definition at line 17816 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fw_index#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::fw_index

Distribution Server's Firmware Image List Index of the image to transfer


Definition at line 17817 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timeout_base#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::timeout_base

Timeout Base to use for the distribution


Definition at line 17819 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_mode#

uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::transfer_mode

BLOB Transfer Mode to use for transferring the image


Definition at line 17820 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h