Data structure of the upload_oob_start_uri event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::elem_index

Server model element index


Definition at line 17612 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::client_address

Address of the Distribution Client


Definition at line 17613 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uri#

uint8array sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::uri

URI to use for retrieving a new firmware image


Definition at line 17614 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h