Data structure of the upload_start_metadata event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::elem_index

Server model element index


Definition at line 17485 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::client_address

Address of the Distribution Client


Definition at line 17486 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

metadata#

uint8array sl_btmesh_evt_fw_dist_server_upload_start_metadata_s::metadata

Metadata of the FW


Definition at line 17487 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h