Data structure of the upload_start_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_start_req_s::elem_index
Server model element index
Definition at line
17508
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_start_req_s::client_address
Address of the Distribution Client
Definition at line
17509
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
size#
uint32_t sl_btmesh_evt_fw_dist_server_upload_start_req_s::size
Upload size
Definition at line
17510
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_server_upload_start_req_s::blob_id
BLOB ID
Definition at line
17511
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fwid#
uint8array sl_btmesh_evt_fw_dist_server_upload_start_req_s::fwid
FWID of the firmware image
Definition at line
17512
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h