Data structure of the update_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_update_client_update_status_s::elem_index
Client model element index
13221
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_update_client_update_status_s::server_address
Unicast address of the server
13222
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_fw_update_client_update_status_s::status
Enum sl_btmesh_fw_update_server_update_status_t. Status code returned
13223
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
phase#
uint8_t sl_btmesh_evt_fw_update_client_update_status_s::phase
Enum sl_btmesh_fw_update_server_update_phase_t. Phase of the Update Server
13226
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
additional_information#
uint8_t sl_btmesh_evt_fw_update_client_update_status_s::additional_information
Enum sl_btmesh_fw_update_client_additional_info_t. Additional information about what will happen to the node after the update is applied. 0 = no changes to DCD; 1 = DCD will change but Composition Data Refresh is not supported; 2 = DCD change and Composition Data Refresh is supported; 3 = node will become unprovisioned.
13229
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_timeout_base#
uint16_t sl_btmesh_evt_fw_update_client_update_status_s::update_timeout_base
Base value for BLOB Transfer Timeout
13240
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
distributor_ttl#
uint8_t sl_btmesh_evt_fw_update_client_update_status_s::distributor_ttl
TTL used by the Distributor. Ignore if no update is active.
13242
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_update_client_update_status_s::blob_id
BLOB ID of the firmware being transferred. Ignore if no update is active.
13244
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint8_t sl_btmesh_evt_fw_update_client_update_status_s::fw_index
Index of the firmware being updated on the node.
13247
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h