Data structure of the update_start_req event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::elem_index

Server model element index


Definition at line 15915 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_update_server_update_start_req_s::client_address

Address of the Update Client


Definition at line 15916 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_fw_update_server_update_start_req_s::blob_id

BLOB ID of the firmware being transferred.


Definition at line 15917 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fw_index#

uint8_t sl_btmesh_evt_fw_update_server_update_start_req_s::fw_index

Index of the firmware to update


Definition at line 15919 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

metadata#

uint8array sl_btmesh_evt_fw_update_server_update_start_req_s::metadata

Metadata for the FWID in the following update_start_req event. May be zero-length.


Definition at line 15920 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h