Data structure of the state_recall event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_generic_server_state_recall_s::elem_index

Server model element index


Definition at line 5935 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

model_id#

uint16_t sl_btmesh_evt_generic_server_state_recall_s::model_id

Server model ID


Definition at line 5936 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transition_time_ms#

uint32_t sl_btmesh_evt_generic_server_state_recall_s::transition_time_ms

Time (in milliseconds) remaining before transition from current state to target state should be complete. Ignored if no transition is taking place.


Definition at line 5937 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

type#

uint8_t sl_btmesh_evt_generic_server_state_recall_s::type

Model-specific state type, identifying the kind of state reported in the state change event. See get state types list for details.


Definition at line 5941 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

parameters#

uint8array sl_btmesh_evt_generic_server_state_recall_s::parameters

Model state - specific parameters, serialized into a byte array


Definition at line 5945 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h