Data structure of the block_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_server_block_complete_s::elem_index
The server model element index.
Definition at line
11442
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_mbt_server_block_complete_s::client_address
The address of the MBT Client.
Definition at line
11443
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_mbt_server_block_complete_s::blob_id
The ID of the BLOB.
Definition at line
11444
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_number#
uint16_t sl_btmesh_evt_mbt_server_block_complete_s::block_number
The index number of the completed block.
Definition at line
11445
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_size#
uint16_t sl_btmesh_evt_mbt_server_block_complete_s::block_size
The size of the completed block.
Definition at line
11446
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h