Data structure of the transfer_start_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_server_transfer_start_req_s::elem_index
The server model element index.
Definition at line
11345
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_mbt_server_transfer_start_req_s::client_address
The address of the MBT Client.
Definition at line
11346
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_mbt_server_transfer_start_req_s::blob_id
The ID of the BLOB.
Definition at line
11347
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_size#
uint32_t sl_btmesh_evt_mbt_server_transfer_start_req_s::blob_size
The size of the BLOB.
Definition at line
11348
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_size_log#
uint8_t sl_btmesh_evt_mbt_server_transfer_start_req_s::block_size_log
The block size as an exponent n in 2^n.
Definition at line
11349
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_mode#
uint8_t sl_btmesh_evt_mbt_server_transfer_start_req_s::transfer_mode
Transfer mode: 1 = Push Mode (client-driven), 2 = Pull Mode (server-driven).
Definition at line
11350
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h