sl_btmesh_evt_node_local_dcd_data#

Event reporting queried composition data page contents.

The contents are requested using the sl_btmesh_node_get_local_dcd command. More than one event may be generated. Page contents are terminated by a sl_btmesh_evt_node_local_dcd_data_end event. Note that the interpretation of the received data is page-specific. Page 0 contains the element and model layout of the node.

Modules#

sl_btmesh_evt_node_local_dcd_data_s

Macros#

#define

Identifier of the local_dcd_data event.

Typedef Documentation#

sl_btmesh_evt_node_local_dcd_data_t#

typedef struct sl_btmesh_evt_node_local_dcd_data_s sl_btmesh_evt_node_local_dcd_data_t

Definition at line 944 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_node_local_dcd_data_id#

#define sl_btmesh_evt_node_local_dcd_data_id
Value:
0x141400a8

Identifier of the local_dcd_data event.


Definition at line 933 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h