sl_btmesh_evt_node_input_oob_request#
The Provisioner is displaying an out of band authentication value.
The application on the node should provide the value to the Bluetooth mesh stack using the sl_btmesh_node_send_input_oob_request_response command.
Modules#
sl_btmesh_evt_node_input_oob_request_s
Typedefs#
Macros#
#define
sl_btmesh_evt_node_input_oob_request_id 0x051400a8
Identifier of the input_oob_request event.
Typedef Documentation#
sl_btmesh_evt_node_input_oob_request_t#
typedef struct sl_btmesh_evt_node_input_oob_request_s sl_btmesh_evt_node_input_oob_request_t
Definition at line
586
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_node_input_oob_request_id#
#define sl_btmesh_evt_node_input_oob_request_idValue:
0x051400a8
Identifier of the input_oob_request event.
Definition at line
574
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h