Data structure of the input_oob_request event.

Public Attributes#

uint8_t

Public Attribute Documentation#

input_action#

uint8_t sl_btmesh_evt_node_input_oob_request_s::input_action

Enum sl_btmesh_node_oob_input_action_t. Selected input action


Definition at line 581 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

input_size#

uint8_t sl_btmesh_evt_node_input_oob_request_s::input_size

Size of data in the input in characters.


Definition at line 583 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h