sl_btmesh_evt_prov_initialization_failed#
Provisioner has not been initialized successfully and is not operational.
It is not possible to use the device as a Provisioner. See the result code for details.
Modules#
sl_btmesh_evt_prov_initialization_failed_s
Typedefs#
Macros#
#define
sl_btmesh_evt_prov_initialization_failed_id 0x1b1500a8
Identifier of the initialization_failed event.
Typedef Documentation#
sl_btmesh_evt_prov_initialization_failed_t#
typedef struct sl_btmesh_evt_prov_initialization_failed_s sl_btmesh_evt_prov_initialization_failed_t
Definition at line
2709
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_prov_initialization_failed_id#
#define sl_btmesh_evt_prov_initialization_failed_idValue:
0x1b1500a8
Identifier of the initialization_failed event.
Definition at line
2699
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h