sl_btmesh_evt_prov_oob_display_input#

Random OOB input data was generated and should be displayed to and input with the device.

Modules#

sl_btmesh_evt_prov_oob_display_input_s

Macros#

#define

Identifier of the oob_display_input event.

Typedef Documentation#

sl_btmesh_evt_prov_oob_display_input_t#

typedef struct sl_btmesh_evt_prov_oob_display_input_s sl_btmesh_evt_prov_oob_display_input_t

Definition at line 2511 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_prov_oob_display_input_id#

#define sl_btmesh_evt_prov_oob_display_input_id
Value:
0x081500a8

Identifier of the oob_display_input event.


Definition at line 2483 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h