Data structure of the model_status event.
Public Attribute Documentation#
server#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::server
Server address.
Definition at line
3924
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::status
Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.
Definition at line
3925
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::elem_index
Element index of model to configure.
Definition at line
3927
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
vendor_id#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::vendor_id
Vendor ID of model to configure.
Definition at line
3928
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
model_id#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::model_id
Model ID of model to configure.
Definition at line
3929
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::value
Extended packet size to set, currently 1 to use extended 0 to not
Definition at line
3930
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h