Data structure of the network_pdu_status event.

Public Attributes#

uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::server

Server address.


Definition at line 3956 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::status

Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.


Definition at line 3957 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

pdu_max_size#

uint16_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::pdu_max_size

Network PDU max size


Definition at line 3959 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h