Sample Breakout Board Configuration
Functions and definitions specific to the breakout board. More...
Macros | |
#define | halInternalInitRadioHoldOff() |
Radio HoldOff not supported. More... | |
#define | halInternalPowerUpBoard() |
#define | halInternalPowerDownBoard() |
#define | DEFINE_SPI_CONFIG_VARIABLES() |
Initialize GPIO powerup configuration variables. More... | |
#define | COM_RETARGET_SERIAL |
Packet Trace | |
PRO2+ SPI-Master configuration When PACKET_TRACE is defined, ::GPIO_PACFGH will automatically be setup by halInit() to enable Packet Trace support on PA4 and PA5, in addition to the configuration specified below.
| |
#define | PACKET_TRACE |
This define does not equate to anything. It is used as a trigger to enable Packet Trace support on the breakout board (dev0680). More... | |
Detailed Description
Functions and definitions specific to the breakout board.
Macro Definition Documentation
#define COM_RETARGET_SERIAL |
GPIO definitions for WSTK BC serial Initialize GPIOs direction and default state for VCP.
Definition at line 119
of file ezr32.h
.
#define DEFINE_SPI_CONFIG_VARIABLES | ( |
| ) |
Initialize GPIO powerup configuration variables.
Definition at line 81
of file ezr32.h
.
#define halInternalInitRadioHoldOff | ( |
| ) |
Radio HoldOff not supported.
Definition at line 64
of file ezr32.h
.
#define halInternalPowerDownBoard | ( |
| ) |
Definition at line 72
of file ezr32.h
.
#define halInternalPowerUpBoard | ( |
| ) |
Definition at line 66
of file ezr32.h
.
#define PACKET_TRACE |
This define does not equate to anything. It is used as a trigger to enable Packet Trace support on the breakout board (dev0680).
Definition at line 59
of file ezr32.h
.