EventActions Struct Reference
The static part of an event. Each event can be used with only one event queue. More...
#include <
ember-types.h
>
Data Fields | |
struct EventQueue_s * | queue |
void(* | handler )(struct Event_s *) |
void(* | marker )(struct Event_s *) |
const char * | name |
The static part of an event. Each event can be used with only one event queue.
Definition at line 436
of file ember-types.h
.
Field Documentation
void(* EventActions::handler) (struct Event_s *) |
Definition at line 438
of file ember-types.h
.
void(* EventActions::marker) (struct Event_s *) |
Definition at line 439
of file ember-types.h
.
const char* EventActions::name |
Definition at line 440
of file ember-types.h
.
struct EventQueue_s* EventActions::queue |
Definition at line 437
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h